Find a partner

Products and Services
Total results: 12 partners
Showing partners per page

Bluewind

Bluewind, an independent engineering company, provides innovative product design solutions in the fields of Electronics, Energy Efficiency, and Connected Devices.

The R&D task force consists of 20+ experienced engineers, providing full product design and covering the complete design cycle: product strategy, hardware and software design, testing, CE compliance, and production.

Founded in 1998, the company serves primary industries located throughout Europe and the USA, offering wide experience over several application fields.

(#STM32CubeAI)

Cartesiam

Cartesiam is an expert in Artificial Intelligence at the Edge. We are an ISV expert in mathematics, AI and signal processing on microcontrollers. Cartesiam, invented NanoEdge™, a revolutionary technology enabling Machine Learning and AI analysis in small footprint, low energy devices, such as STM32 microcontrollers.

This capability is unique in the market as it enables not only analysis, but also learning directly within the microcontroller and this, without the help of a complex cloud infrastructure. 

Devices equipped with NanoEdge AI™ can autonomously learn from their environment, identify anomalies, and send alerts. 

(#STM32CubeAI)

Imagimob

Imagimob is a global leader in artificial intelligence products for STM32. Based in Stockholm, Sweden, the company has been serving customers within the automotive, manufacturing, healthcare and lifestyle industries since 2013. The experienced and visionary team that makes up Imagimob is tirelessly dedicated to staying on top of the latest research, thinking new, and thinking big.

(#STM32CubeAI)

Inventhys

Inventhys is a fast-growing, end-to-end IoT development services company. Our engineers design hardware, embedded software, mobile apps and cloud systems. 

This unique combination of expertise ensures integrated and coherent design and project management. We help our customers from concept to mass production, including regulatory certification. 

Our customers are start-ups in France and Silicon Valley, and large / very large accounts.

Our offices are in Annecy, Grenoble and San Francisco.

(#STM32CubeAI)

Lenord + Bauer

Lenord + Bauer is an internationally active specialist for motion sensors and integrated drive technology. 

Lenord + Bauer develop, produce and distribute leading technological solutions for mobility and machinery industries.

The focus is on the railway industry, machine tools and packaging machine applications. For more than 50 years the customers benefit from our high technical advisory expertise and specialist knowledge in the customer application. 

Lenord + Bauer is certified according to DIN EN ISO 9001 and 14001, as well as IRIS.  

Lenord + Bauer coorperates with STMicroelectronics to satisfy increasing customer demands regarding KI, condition monitoring and predictive maintenance  (#STM32CubeAI).

NALBI

NALBI is an AI company focusing on deep learning-based computer vision technology in embedded systems. 

Our core competencies are highly optimized deep learning models and a computing engine specially optimized for the target device. 

(#STM32CubeAI)

Neovision

Neovision provides engineering consultancy in artificial intelligence. Our fields of expertise encompass image recognition, natural language processing, predictive analysis and data mining for complex task like human activity detection, quality control, help in the decision-making process, automation, massive data analysis… Not only do we provide bespoke and innovative solutions, but we can also guarantee you will get evolving and ready-to-use technology (#STM32CubeAI).

Octonion

Octonion is an IoT Intelligent Edge software platform that has built an unprecedented AI framework at the Edge. The platform is a end to end IoT software solution with 3 layers: firmware, gateway and Cloud. The platform runs on any 32-bit Arm®-based Cortex®-M microcontrollers and is optimized for STM32 chipset. 

Octonion platform has 3 key assets: AI at the Edge, Security at the Edge and Connectivity. Octonion’s expertise allows Customers to deploy a connected project in 6 months as opposed to the 18 to 24 months currently needed with most other IoT platforms.

(#STM32CubeAI)

 

Qeexo

Qeexo develops machine learning solutions to generate actionable insights from sensor data. 

The company works with leading device OEMs and component manufacturers to power new and exciting user experiences on over 150 million devices worldwide. In industries such as mobile, IoT, and automotive, there are billions of devices where computation and memory are highly constrained. 

Qeexo's proprietary, low-latency, low-power models are engineered to have an incredibly small footprint - ideal for making high-accuracy predictions in these environments.

(#STM32CubeAI)

SensiML

SensiML offers cutting-edge development software that transforms low power IoT endpoints into intelligent AI devices delivering meaningful sensor insights. The company’s flagship solution, the SensiML Analytics Toolkit, provides a complete embedded algorithm development workflow spanning data collection, labeling, testing, algorithm and firmware auto generation.  SensiML can be effectively used by teams with or without data science expertise to rapidly build intelligent IoT endpoint devices.

(#STM32CubeAI)

SIANA Systems

Siana-Systems has particular expertise in embedded applications (firmware) that utilize common wireless standards/protocols and interfaces such as Z-Wave, Zigbee, ISM band radios, BTLE, Bluetooth Classic and Wi-Fi.

Key areas of application specializations are embedded systems focused on: consumer, audio and gaming accessories, Medical (low power and high performance/reliability), home/industrial automation, wearable low-power embedded devices, remote firmware update over networks and wireless standards, cloud connected, remote device network partition and over-the-air firmware upgrade, distributed and mesh embedded networks, low-power instrumentation (+ sensors), sporting/wearable monitoring, embedded graphics applications and Intelligent Artificial applications (#STM32CubeAI).

STATWORX

STATWORX is a consulting company for data science, machine learning, and AI located in Frankfurt, Vienna and Zurich. We support our clients in the development and implementation of cutting-edge data science and machine learning projects as well as data driven products.

We offer an exhaustive end-2-end data consulting approach to support our clients with:

  • Data Strategy (eg. use case ideation, change management, organizational setup support)
  • Data Engineering (design and implementation of data pipelines, storages and architectures)
  • Data Science (development, training and evaluation of machine learning and AI models)
  • Data Operations (implementation and operation of machine learning models)
  • Data Academy (assuring knowledge development through standardized as well as custom tailored trainings and workshops)

In our partnership with ST, we support you in the development and integration of deep learning and neural network solutions for the STM32 microcontroller family (#STM32CubeAI)



Support & Feedback