Find a partner

Products and Services
Total results: 9 partners
Showing partners per page

Actility

Actility is a global supplier of IoT connectivity solutions. Combining best-in-class LoRaWAN network servers with device & network management and added value services. Actility helps operators and enterprises to deploy IoT solutions for addressing vertical industries such as smart cities, logistics or the Industry 4.0. 

With more than 100 million dollars raised in funding, Actility is the leader in LoRaWAN network deployments with more than 40 global clients including Orange, Proximus, KPN or Swisscom. 

(#LoRaStarterPacks) (#STSECURE) (#STSAFE-A)

AWS

AWS IoT is a managed cloud platform that lets connected devices easily and securely interact with cloud applications and other devices. AWS IoT can support billions of devices and trillions of messages, and can process and route those messages to AWS endpoints and to other devices reliably and securely. With AWS IoT, your applications can keep track of and communicate with all your devices, all the time, even when they aren’t connected.

STMicroelectronics is Standard Technology Partner in the AWS Partner Network (APN).
 
(#STSAFE-A) (#STSAFE-J) (#STSAFE-TPM) (#STSECURE)
 

JORJIN

Jorjin Technologies is a provider of modular processing, sensing and wireless connectivity solutions, which enable our customers to bring innovative products to market fast with competitive cost. Jorjin wireless system in package (SiP) modules targeting wearable consumer electronics, automotive infotainment, cloud connected devices, and industrial mobile computing market. 

Jorjin cover wide range of protocols including Wi-Fi, Bluetooth, ZigBee, WiSun, NFC, GPS, and GLONASS. In addition to supplying hardware, Jorjin offers driver porting services onto a wide range of application processors; Jorjin as well provide MCU-based connectivity solutions to support the emerging Internet of things (IoT) market. Jorjin hold advanced technology: producing extremely small footprints modules using either package on package (PoP) or multi-chip module (MCM) assembly technique. 

Jorjin recently also set up a new imaging team to design and supply a range of camera sensor modules, 3D time of flight cameras and other sensor solutions to build up smart glasses for various industries applications.

(#STSAFE-A) (#STSECURE)

 

Microsoft

Transform your business with Internet of Things.
Build things : IoT begins with your things. Build with your things, from adding sensors to creating smart devices, to start your IoT solution.
Control your things : Deploy IoT solutions that control, monitor, and manage your things, allowing you to capture real-time data. 
Analyze data : Take the data you collect and apply advanced analytics to uncover new business insights. 
Act on insights : Transform insights into action through powerful applications—creating new revenue and business opportunities.

(#STSAFE-A) (#STSAFE-J) (#STSAFE-TPM) (#STSECURE)

Mocana

Mocana’s end-to-end cybersecurity system protects millions of industrial control systems and smart connected devices that comprise the Internet of Things across all sectors.

"Mocana" means to set free, and our mission is to protect countries, cities, and families by enabling devices of every kind to be trustworthy and run securely and freely. Mocana was founded in 2002 to help protect military aircraft, vehicles, and devices. Our security software protects devices by using cryptography designed to run on microcontrollers and embedded devices. Today, we serve both the defense and commercial sectors.

Mocana is now running on every type of device you can imagine: fighter jets, helicopters, tanks, commercial aircraft, industrial automation and controls, thermostats, surveillance cameras, network gateways, set top boxes, medical devices, and much more. In fact, we now protect more than 100 million devices.

200 of the largest industrial manufacturing, aerospace, defense, utilities, energy, and transportation companies trust Mocana to harden their mission-critical devices and secure IoT communications using Mocana TrustPoint, our embedded IoT endpoint software, and Mocana TrustCenter, our automated security services platform. Our solutions enable our customers to secure their manufacturing supply chain.

Together, let's secure the Internet of Things from the inside out.

(#STSAFE-A) (#STSAFE-J) (#STSAFE-TPM) (#STSECURE)

MXCHIP

Headquartered in Shanghai, MXCHIP Information is a wireless systems solution company with the unique wireless products for IoT Application. Founded in 2004, MXCHIP Information has created the mature wireless technology that has gone into the creation of lower power, safety, and high performance products for wireless applications.
MXCHIP Information was focused on the embedded system development from 2007. Subsequently, it has launched multiple diversified wireless modules based on STM32 MCU widely covering specific vertical market segments including Smart Home, Smart Building, Smart Lighting and Industrial etc. MXCHIP Information was the first in the industry to launch the Micro-Controller based Internet Connectivity Operating System, namely MiCO which can help developer flexibly design their smart products with creative ideas. In 2013, it has launched EMW3165 integrated STM32F411, pretty popular in market with more than 1 million shipment breakthrough. In 2017, it is the latest launched EMB1061 using ST BlueNRG-1 to enable the wireless monitoring and control of utility and industrial systems.
MXCHIP Information spans the complete end-to-end wireless solution and includes an extensive product portfolio on wireless modules, IoT Operating System MiCO, Mobile Application Development and Cloud Service platform as for 3rd party access to public cloud or protocol access, etc. The company’s single-stop approach enables MXCHIP Information to deliver an optimal wireless solution to meet customer’s requirements at an optimal benchmark point. Our mission is connecting the unconnected to enable our life smarter, simpler and more wonderful.

(#STSAFE-A) (#STSECURE))

Prove & Run

Prove & Run was created with the idea that large-scale deployments of connected devices is an attractive target for remote cyberattacks and that the solutions used in the mobile industry are not sufficient to answer to the challenge. Prove & Run answers to the cybersecurity requirements of the device OEMs at all steps of their product life-cycle by providing: 

• Security consulting services such as performing security analysis, defining security architecture and security requirements

• Solutions to secure-by-design their devices

When designing connected devices, security engineers can rely on three pillars:

1. Secure Elements

2. Trusted Execution Environments (TEE) or secure OSs

3. Hardware- or software-based hypervisors

In order to resist to sophisticated remote attacks, Prove & Run has designed TEEs and hypervisors that are highly resistant against hackers and as close as possible to zero bugs and that can be used in complement to the Secure Elements to secure by-design the OEM's devices. 

(#STM32MPU) (#STM32MP1) (#STSAFE-A) (#STSAFE-J) (#STSAFE-TPM) (#STSECURE)

Sigfox

Sigfox, it’s about connecting the unconnected! 

An inexpensive, long distance and lower power solution that's primed for multiple industrial & consumer applications.

Through its global LPWA network and rich ecosystem of expert partners, Sigfox delivers out-of-the box, two-way, secured communication services to unlock the true potential of the Internet of Things (IoT).

Sigfox provides a standard way of collecting data from sensors and devices with a single, standard-based set of APIs.

Besides, the Sigfox disruptive technology complements traditional cellular M2M by enabling global, ubiquitous, ultra-long battery life solutions at the lowest cost.

(#STSAFE-A) (#STSECURE)

 

wolfSSL

wolfSSL focuses on creating high quality, portable, embedded security software targeted at IoT, embedded, and RTOS environments. Speed, size, portability and robust security make wolfSSL the best SSL/TLS option for securing your connectivity. 

Current products include the wolfSSL embedded SSL library, wolfCrypt embedded crypto engine with FIPS 140-2 certification, wolfMQTT, wolfBoot secure bootloader, wolfSSH, wolfTPM 2.0, and wolfSSL JNI wrapper. wolfSSL is the first commercial implementation of TLS 1.3.

(#STSAFE-A) (#STSAFE-J) (#STSAFE-TPM) (#STSECURE)