Find a partner

Products and Services
Total results: 5 partners
Showing partners per page

AWS

AWS IoT is a managed cloud platform that lets connected devices easily and securely interact with cloud applications and other devices. AWS IoT can support billions of devices and trillions of messages, and can process and route those messages to AWS endpoints and to other devices reliably and securely. With AWS IoT, your applications can keep track of and communicate with all your devices, all the time, even when they aren’t connected.

STMicroelectronics is Standard Technology Partner in the AWS Partner Network (APN).
 
(#STSAFE-A) (#STSAFE-J) (#STSAFE-TPM) (#SecureMCUs)
 

Microsoft

Transform your business with Internet of Things.
Build things : IoT begins with your things. Build with your things, from adding sensors to creating smart devices, to start your IoT solution.
Control your things : Deploy IoT solutions that control, monitor, and manage your things, allowing you to capture real-time data. 
Analyze data : Take the data you collect and apply advanced analytics to uncover new business insights. 
Act on insights : Transform insights into action through powerful applications—creating new revenue and business opportunities.

(#STSAFE-A) (#STSAFE-J) (#STSAFE-TPM) (#SecureMCUs)

Mocana

Mocana’s end-to-end cybersecurity system protects millions of industrial control systems and smart connected devices that comprise the Internet of Things across all sectors.

"Mocana" means to set free, and our mission is to protect countries, cities, and families by enabling devices of every kind to be trustworthy and run securely and freely. Mocana was founded in 2002 to help protect military aircraft, vehicles, and devices. Our security software protects devices by using cryptography designed to run on microcontrollers and embedded devices. Today, we serve both the defense and commercial sectors.

Mocana is now running on every type of device you can imagine: fighter jets, helicopters, tanks, commercial aircraft, industrial automation and controls, thermostats, surveillance cameras, network gateways, set top boxes, medical devices, and much more. In fact, we now protect more than 100 million devices.

200 of the largest industrial manufacturing, aerospace, defense, utilities, energy, and transportation companies trust Mocana to harden their mission-critical devices and secure IoT communications using Mocana TrustPoint, our embedded IoT endpoint software, and Mocana TrustCenter, our automated security services platform. Our solutions enable our customers to secure their manufacturing supply chain.

Together, let's secure the Internet of Things from the inside out.

(#STSAFE-A) (#STSAFE-J) (#STSAFE-TPM) (#SecureMCUs)

Prove & Run

Prove & Run’s was founded in 2009 and is a rapidly growing software company whose mission is to help its customers resolve the cybersecurity challenges linked to the large scale deployment of connected devices and of the Internet of Things. 

The main source of cybersecurity issues can be attributed to either improper security measures or faulty software where defects in either the software architecture, design, implementation or configuration create vulnerabilities that can be potentially exploited for attacks. The challenge is therefore to produce software as close as possible to zero-defects as possible. In the remainder the term “security” will be used as a synonym to “cybersecurity”. 

We provide cost effective, highly secured, off-the-shelf TEE and hypervisors that dramatically improve the level of security of connected systems:

  • ProvenCore: a formally proven OS kernel. It is a new generation ultra secure TEE. ProvenCore is typically used for running security critical applications (FOTA, VPN, Firewalls, Authentication, etc.) and security protection of existing non-secure OS. ProvenCore is available on Arm Cortex-A and Cortex-M architectures.
  • ProvenVisor: a formally proven secure hypervisor. It is a new generation ultra secure hypervisor. ProvenVisor is typically used for secure isolation of existing OS and legacy SW stack.  ProvenVisor is available on ARM Cortex-A architectures.

While ProvenCore and/or ProvenVisor can be used on their own or in combination to secure any IoT architecture, in most of the cases, the use of single instance of ProvenCore on a given IoT architecture will be sufficient in order to be protected against hackers with multi-million Dollars budgets for the identification phase.

This is derived from the fact that the security properties of ProvenCore and ProvenVisor have been formally proven, down to the generated code. That insures that they are going to be as close as possible to zero-defaults and therefore highly resistant to attacks. 

(#STM32MPU) (#STM32MP1) (#STSAFE-A) (#STSAFE-J) (#STSAFE-TPM) (#SecureMCUs)

wolfSSL

wolfSSL focuses on creating high quality, portable, embedded security software targeted at IoT, embedded, and RTOS environments. Speed, size, portability and robust security make wolfSSL the best SSL/TLS option for securing your connectivity. 

Current products include the wolfSSL embedded SSL library, wolfCrypt embedded crypto engine with FIPS 140-2 certification, wolfMQTT, wolfBoot secure bootloader, wolfSSH, wolfTPM 2.0, and wolfSSL JNI wrapper. wolfSSL is the first commercial implementation of TLS 1.3.

(#STSAFE-A) (#STSAFE-J) (#STSAFE-TPM) (#SecureMCUs)



Support & Feedback