Find a partner

Products and Services
Total results: 298 partners
Showing partners per page

Savoir-Faire Linux

Savoir-faire Linux is a global reference for any open source software integration. Our clients rely on us for consulting, integration, development, training and IT support services. Our broad expertise in business, web, infrastructure and embedded solutions make us the ideal partner of choice for many companies and their highly complex projects given our team of more than 50 open source engineering consultants available to meet all varieties of challenges.

Our clients derive from a variety of industries and verticals such as:

• Aeronautics,

• Aerospace

• Automotive OEM's & Tier 2's

• Consulting Agencies,

• IT Security Firms

• Financial Institutions,

• Hardware Manufacturers

• Entertainment Organizations

Savoir-faire Linux is also a major contributor of the following Open source technologies as Linux Kernel, Yocto, Buildroot, Ffmpeg, Zephyr, Jami, OpenDHT. 

SCIOPTA Systems

Founded as Litronic AG in 1988, SCIOPTA Systems AG is based in Bottmingen/Basel (Switzerland). 
Since the inception SCIOPTA Systems AG is specialized in real-time systems. 
SCIOPTA Systems develops, sells, supports and maintains systems software for safety-critical embedded applications.
This includes real-time operating systems, network software, file systems, software for interface bus systems, board support packages and other system software.
SCIOPTA is a message based real-time operating system with many built-in safety functions and is therefore very well suited for software forming part of safety-related systems. SCIOPTA has been certified by TÜV to IEC61508 at Safety Integrity Level 3 (SIL3), EN50128 and ISO 26262.
But SCIOPTA is more than just an RTOS. It is a new and modern approach to design embedded systems. The direct message passing method allows easy and time-saving design of robust and safe systems. Applications based on the SCIOPTA Method can cover small static SoC designs to large dynamic distributed systems.

Scriptr

Scriptr.io reduces the complexity & cost of enterprise IoT and digital transformation by providing a marketplace of ready to use vertical IoT applications backed by an award winning agile, scalable & secure development platform & runtime.  

Scriptr.io is compatible with all major IoT data platforms; IBM IoT, Azure IoT, AWS IoT, and many others to accelerate your industrial and enterprise IoT applications.

Scriptr.io is delivered on demand as a fully managed cloud service, on premise or at the edge.

Secure Thingz

Secure Thingz is the global domain expert in device security, embedded systems, and lifecycle management. 

Since 2018, the company is part of IAR Systems, the future-proof supplier and software tools for embedded development. Secure Thingz is focused on delivering advanced security solutions into the emerging industrial Internet of Things, critical infrastructure, automotive and other markets. The Secure Deploy™ architecture has been developed to solve the major security issues challenging the IoT.

SEGGER Microcontroller

SEGGER Microcontroller is a full-range supplier of software, hardware and development tools for embedded systems. The company offers support throughout the whole development process with affordable, high quality, flexible and easy-to-use tools and components.

SEGGER offers solutions for secure communication as well as data and product security, meeting the needs of the rapidly evolving IoT.

SEGGER was founded in 1992, is privately held, and is growing steadily. Headquartered in Germany, with US offices in the Boston area and Silicon Valley, as well as distributors in all continents, SEGGER offers its full product range worldwide.

(#FuSa)

SensiEDGE

SensiEDGE lowers the barriers to entry for designers developing IoT solutions.

The SensiEDGE off-the-shelf IoT module integrates sensors, micro-controller, RF communication and power management ICs. It simplifies and reduces development time and cost. The IoT System-on-Modules (SoM) BLE, proprietary Sub 1GHz, LoRa and Sigfox enables sensors connectivity to the cloud, packed into a tiny form factor. 

SensiEDGE's gateways, which include BLE, Wi-Fi, 6LoWPAN, LoRa and LTE, simplify cloud connectivity.

SensiEDGE's certified "hardware-ready" & SW package solutions optimizes the ease of building new IoT Product.

SensiML

SensiML offers cutting-edge development software that transforms low power IoT endpoints into intelligent AI devices delivering meaningful sensor insights. The company’s flagship solution, the SensiML Analytics Toolkit, provides a complete embedded algorithm development workflow spanning data collection, labeling, testing, algorithm and firmware auto generation.  SensiML can be effectively used by teams with or without data science expertise to rapidly build intelligent IoT endpoint devices.

(#STM32CubeAI)

Sensory

Sensory, Inc. is a profitable, venture backed, privately held company focused on improving the user experience through embedded machine learning technologies such as voice, vision, and natural language processing.

Seongji Industrial

Founded in 1985, Seongji Industrial Co., Ltd. has grown to provide customers with various interface solutions that transmit information connecting various electronic devices and that communicate with people and machines. As a result, we are now a leading manufacturer of electronic components. Thank you for your constant interest and support.

Until now, we have mainly produced wired electronic components such as harness, PBA and Touch Display, but we have expanded to wireless communication business such as wireless communication module and IoT for the continuous growth of the 4th Industrial Revolution era when all objects are connected to high speed network.

All employees at Seongji are making greater efforts to develop competitive parts and high value-added parts and complete products in order to provide customers with the best value. Through this, we will secure various wired and wireless solutions for CONNECTING, which is the concept of Seongji industry, and open the future we all dream together with our customers.

 

Sequitur Labs

Sequitur Labs delivers security, tooling and process to bring trusted, resilient products to market.

Over 20 billion embedded systems are expected to be connected to the Internet by 2020. From medical devices to self-driving automobiles and industrial robots, these devices will connect people, integrate processes and drive global productivity. These devices will collect and ingest data and feed AI algorithms in order to accelerate and improve decision-making. They are at the heart of a “Smart Future”. McKinsey & Co. measures the economic impact of the connected economy in trillions of dollars over the next decade.

The greatest obstacle to this smart future is—SECURITY. Without the right security framework, each connected device is a target for malicious attacks. The last three years have seen a number of attacks such as Mirai and there will surely be more. Securing connected devices is therefore a prime imperative. So why aren’t companies taking steps to do so? They are. The reality is that securing embedded devices is hard. It’s expensive.

We are working to make it simple, affordable and accessible.

We are your security team.

SIANA Systems

Siana-Systems has particular expertise in embedded applications (firmware) that utilize common wireless standards/protocols and interfaces such as Z-Wave, Zigbee, ISM band radios, BTLE, Bluetooth Classic and Wi-Fi.

Key areas of application specializations are embedded systems focused on: consumer, audio and gaming accessories, Medical (low power and high performance/reliability), home/industrial automation, wearable low-power embedded devices, remote firmware update over networks and wireless standards, cloud connected, remote device network partition and over-the-air firmware upgrade, distributed and mesh embedded networks, low-power instrumentation (+ sensors), sporting/wearable monitoring, embedded graphics applications and Intelligent Artificial applications (#STM32CubeAI).

Sibros

Sibros' Connected Vehicle platform connects and manages all in-vehicle software and data between vehicles, networks and the cloud, from R&D to the last mile. This bi-directional, software first approach helps OEMs deliver never-before-available vehicle functionality and personalized mobility services over-the-air and at scale.

Sigfox

Sigfox, it’s about connecting the unconnected! 

An inexpensive, long distance and lower power solution that's primed for multiple industrial & consumer applications.

Through its global LPWA network and rich ecosystem of expert partners, Sigfox delivers out-of-the box, two-way, secured communication services to unlock the true potential of the Internet of Things (IoT).

Sigfox provides a standard way of collecting data from sensors and devices with a single, standard-based set of APIs.

Besides, the Sigfox disruptive technology complements traditional cellular M2M by enabling global, ubiquitous, ultra-long battery life solutions at the lowest cost.

(#STSAFE-A) (#STSECURE)

 

SIGMADESIGN

Pacific Northwest based SIGMADESIGN partners with you to bring your consumer and industrial Internet of Things (IoT) and mechatronic devices to market with expert capabilities in hardware and firmware design. From wireless communications and MEMS sensor platforms to micro form-factor motorized systems, we enjoy incorporating trusted STMicroelectronics processors, modules, and integrated circuits into our Customers’ products. In fact, STM32 represents the core of our new embedded IoT platform “ARI”, which we can leverage for quick-turn and low-NRE semi-custom board designs to fit your budget.

With firmware, software, electronics, systems, and mechanical engineering along with industrial design, manufacture, assembly, and test facilities all under one roof, SIGMADESIGN can be your end-to-end product design partner. Alternatively, with so much experience with STMicroelectronics components, we can review your PCB designs or code for correctness and regulatory compliance. (FCC/IC, CE, etc.)

 

Simma Software

Simma Software, the CAN experts, speacializes in real-time communication protocols with a focus on CAN software including J1939, UDS, ISO15765, CANopen, and XCP. For almost 15 years, customers all over the world have worked with Simma on projects needing CAN support including the implementation of flash bootloaders. Simma supports all ST microcontrollers including the STM8, STM32 and SPC5 families.

SINNO

We believe in simplicity! Our mission is to solve daily living issues by applying technology in a clever way.
With more than 15 years of experience in development of technology systems for various industries (Automotive, Consumer, Lighting and Aerospace) we offer to our customers solutions that would meet and exceed their targets.
From simple solutions up to complex systems SINNO provides a range of different high quality services with the ultimate goal of customer satisfaction.

  • Technology advisory
  • Hardware/Electronics development
  • Software development
  • Verification and validation
  • Product and prototype builds
  • Coaching and training on several technologies

SMART IN OVATION

The SMART IN OVATION GmbH company, with headquarters in Stuttgart, Germany, has been a supplier of innovative control system and software products and associated services for automotive and industrial clients for more than 30 years.

Technology? Boring? Never! Give your products their own character. Make your company stand out from the competition with innovative solutions – from SMART IN OVATION.

Bring individual solutions that are tailor-made for your tasks to life with our help. Benefit from our experience and impress your customers with cost-effective, tailored solutions, state-of-the-art future-proof technology, groundbreaking operating concepts, reliability, and premium quality.

Four operational divisions – one aim: technology to inspire!

 

Of course we are ISO 9001:2008 certified.

 

 

 

SoMLabs

Flexible SOM modules developer and producer, focused on embedded industrial market. 

SoMLabs is a part of BTC Group, a company in electronics business since 2003. 

SoMLabs is focused on development and manufacturing of a wide range of embedded platforms such as System on Modules (SoM) and Carrier Boards (CB) for embedded projects. 

We are committed to provide SoMs for companies who demand reliable hardware and software solutions for rapid development. (#STM32MPU) (#STM32MP1)

 

Sotronik

The development of customized embedded systems is a core capability of SOTRONIK. Our engineers for hardware-near software development are well trained and have a lot of practical experience, earned by numerous projects with different ST Microcontrollers, STM8 and STM32, over the last 15 years.

Some requirements and topics from these projects are :

  • IoT-Cloud and Industry 4.0 applications using different wireless interfaces (LoRa, WiFi, BLE, NFC ... and others), 
  • Smart connectivity and secure remote access implementations (plug&play), 
  • Tight real-time and high precision control algorithms, 
  • Implementations of various interfaces and industrial communication protocols (Ethernet-based, CAN/CANopen, USB-Host/-Device, Modbus ... and others),
  • "Embedded-Webserver"-implementations on STM32-devices as an option for browser-based visualization and configuration, 
  • Automatic c-code generation from Matlab-Simulink®-models and firmware code integration (RTW-"model-to-code"-approach).

We develop, maintain and support longevity projects (15 years plus) and have also in house resources to automate Production-, Calibration-, and Test- appliances. In addition SOTRONIK has a strong Partner Network for Mechanical Engineering, App and Cloud development for tight solutions.



SPARK Microsystems

SPARK Microsystems is bringing to the world a wireless transceiver that will change the way we think about low-power wireless and that is ready for the Internet of Things revolution: - An order of magnitude better energy efficiency - A shorter latency - A Higher data rate - More robust and secure communications.