Filters

STM32CubeL1

Getting Started Video with STM32Cube.AI (09:19)

Get started with STM32CubeMX software tool on the PC, through a simple example: displaying trace messages on the PC sent via an STM32 Nucleo board via its Virtual COM port facility.

Artificial Neural Network mapping made simple with the STM32Cube.AI (01:48)

The STM32Cube.AI is an extension pack of the widely used STM32CubeMX configuration and code generation tool enabling AI on STM32 Arm® Cortex®-M-based microcontrollers.

Getting started with STM32CubeMX v5.0 (2:07)

Rich by its features-set, STM32CubeMX is changing its skin today to provide to the developers an improved access to the Pinout, Peripherals and Middlewares parameters to ease the configuration and optimized the project development time. This new look is also standardizing the User Interface of the different Software Development Tools of the STM32Cube ecosystem.

How to easily port Low-Layer examples (9:40)

In our continued efforts to simplify developers’ life within the STM32Cube environment, we just introduced a new video demonstrating how to easily port an example built using ST’s new STM32Cube Low-Layer APIs from one board (NUCLEO-L476RG) to another (32L496GDISCOVERY) within the same STM32 family. Using the Low-Layer template project corresponding to the target board, the process can be as simple as copying the applicative code from the original project and pasting it into the template project source files already configured to accommodate the new BSP.

Product Overview - STM32Cube making STM32 development easier (07:19)

A new free software from ST, is simplifying development on STM32, through a consistent set of software: STM32CubeMX, software tool on the PC, generating initialization code, and also a collection of embedded software bricks, abstracting the used STM32 and coming with tons of usage examples !

STM32 Releasing your creativity (01:10)

Check out our video to get inspired to release your creativity


×