electronica-india-2022




electronica India

 

21-23 September 2022 (in-presence show)

 

Find out more

 

Visitor registration

India's and South-Asia's largest conference for electronic components is happening on-site at Greater Noida, from 21- 23 September, 2022

The event is an excellent opportunity to share insights around revolutionary technologies and ambitious strategies. It will foster insightful conversations and collaboration around electronic components, systems, applications, and solutions.

TOPICS

Powering your innovation

STMicroelectronics will take part in the 2022 edition of the International Trade Fair for Electronic Components, Systems, Applications and Solutions Design.

Join us at this event to discover new emerging and sustainable technologies and applications from ST.

Visit ST booth - SB 15, Hall 11

Our booth will show advanced ST technologies and solutions /innovations on
  • Smart Mobility
  • Power & Energy
  • STM32 ecosystem & graphics
  • IoT & Connectivity

We look forward to showcasing proof of concepts at the Innovation Zone. Together with our partners, we’re powering your next design innovation!

WHAT YOU WILL SEE

Key demos covering 4 broad areas:

Smart Mobility

  • Traction inverter

Reference board suitable for 320~420V & 50KW continuous power for three-phase PMSM traction applications. This solution is based on the 32-bit automotive-grade microcontroller SPC58NN, which offers a software resolver and decoder algorithm to minimize external components. The on-board SiC MOSFET, gate driver L9502 / STGAP & SBC L9396 boost power efficiency.

  • On-board charger (3.3kW)

This reference design is built around the automotive microcontroller SPC58NN and six Power MOSFETs. Targeting input range 176~264V AC 50Hz and to charge battery of plug-in HEVs and EVs between 260~420Volt DC, this reference solution features a bridge interleaved PFC & FB LLC topology.

  • 6kW wide range LLC converter

6kW DC-DC Converter based on LLC topology. It is used in EV infrastructures and battery charging applications.

  • 2500W LEV charger

Charger module for light electric vehicle

 

Power and Energy

  • USB Type-C™ and Power Delivery

Flexible and robust solutions for certified source and sink

One cable to rule them all
Today, an increasing number of devices and applications are adopting USB Type-C connectors for many good reasons:
  • With reversible plugs, it can be plugged into a device both sides of the cable;
  • Can carry up to 100W of charging power (from 5V/0.5A up to 20V/5.0A);
  • t merges both legacy Type-A and -B functions in a single port and can even change roles on the fly.

New products for new applications
In addition to complying with USB I/F requirements, application-specific features are mandatory to ensure safe operation with the correct protection level, regardless of the use case.
As every USB Type-C implementation is application specific, ST offers several reference designs to reduce development time and costs.
Read our blog post: Moving to USB-C, The STUSB45 and Its Reference Design in a Video 
Discover our USB Type-C and Power Delivery Controllers

  • ST Power Devices

GaN Family – VIPerGaN50 / MasterGaN1 and ST-One Devices

The VIPERGAN50 is a high voltage converter, designed for medium power quasi-resonant ZVS (Zero Voltage Switching at switch turn-on) flyback converters, capable to provide an output power up to 50 W in wide range. It integrates a complete set of features that provide an extremely flexible and easy to use chip and helps to design a highly efficient offline power supply.


The ZVS quasi-resonant operation with the dynamic blanking time feature and the valley synchronization function, that turns on the power switch always at the valley of the drain resonance, reduces the switching losses and maximizes the overall efficiency at any input line and load condition. The advanced power management with the low quiescent helps to achieve low stand-by consumptions. The feed-forward compensation minimizes the maximum output peak power variation over the entire input voltage range.


In addition to the above functions, the device offers protection features that considerably increase end-product’s safety and reliability: the output overvoltage protection, the overtemperature protection (OTP), the overload protection (OLP), the brown-in/out protection, that set the input voltage level to power on and power off the converter and the input overvoltage protection (iOVP), that protects the system in case of an abnormal increase of the input line. All the protections are auto-restart mode.

The MASTERGAN1 is an advanced power system-in-package integrating a gate driver and two enhancement mode GaN transistors in half‑bridge configuration. The integrated power GaNs have RDS(ON) of 150 mΩ and 650 V drain‑source breakdown voltage, while the high side of the embedded gate driver can be easily supplied by the integrated bootstrap diode.


The MASTERGAN1 features UVLO protection on both the lower and upper driving sections, preventing the power switches from operating in low efficiency or dangerous conditions. The interlocking function avoids cross-conduction conditions.


The input pins extended range enables an easy interfacing with microcontrollers, DSP units or Hall effect sensors.
The MASTERGAN1 operates in the industrial temperature range, from -40 to 125°C.
The device is available in a compact 9 x 9 mm QFN package.

The ST-ONE is the world’s first digital controller embedding an Arm® Cortex® M0+ core, an offline programmable controller with synchronous rectification, and USB PD PHY in a single package. It is designed to control ZVS non-complementary active clamp flyback converters to create high-power density chargers and adapters with USB-PD interface.


The device includes an active clamp flyback controller and its HV startup on the primary side, a microcontroller and all the peripherals required to control the conversion and the USB-PD communication on the secondary side. The two sides are connected through an embedded galvanically-isolated dual communication channel. By using a novel non-complementary control technique and specifically designed power modes the device allows to reach both high efficiency and low no load power consumption.


The device is delivered with a pre-loaded firmware, which handles the power conversion and the communication protocols for USB-PD, including optional PPS and electronically-marked cable management.

A dedicated memory stores a default device configuration during factory process. The user can change or adapt this memory area to fit the final product specifications.

  • 3kW high density and high efficiency telecom rectifier solution

STDES-3KWTLCP - 3 kW telecom rectifier reference design based on the STM32G474RBT6 digital power MCU

The STDES-3KWTLCP is a 3 kW AC-DC converter designed for telecom rectifier applications. This type of application requires high efficiency over the entire load operating range and across the universal mains input voltage range.


This reference design paves the way to a compact solution (up to 40 W/inch3), offering a high peak efficiency (96.3%), low THD distortion (less than 5% THD at full load), and a reduced bill of materials.

The system consists of two power stages: a bridgeless totem-pole PFC controlled by an STM32G474RBT6 and an isolating regulation stage implemented with a full-bridge LLC with zero-voltage-switching (ZVS) PWM, and synchronous rectification (SR) controlled by a second STM32G474RBT6 microcontroller.

The STDES-3KWTLCP also helps you to design an innovative topology with the latest ST power kit devices: silicon carbide MOSFETs, high-voltage MDmesh MOSFETs, STripFET MOSFETs, isolated FET drivers, and a VIPer converter.
The STDES-3KWTLCP is a fully assembled kit developed for performance evaluation only, not available for sale.

  • 5 kW low voltage high current inverter for industrial motor control applications 

The STEVAL-CTM009V1 evaluation kit for motor control is used for testing the features of ST Power MOSFETs based on STripFET™ F7 technology. The 100 V STripFET™ F7 devices (STH31*N10F7) are ideal for low voltage (up to 48 V), high current applications such as forklifts, golf carts and power tool. The STEVAL-CTM009V1 kit is composed of the STEVAL-CTM004V1, STEVAL-CTM005V1, STEVAL-CTM006V1, STEVAL-CTM008V1 boards which have to assembled together to build an inverter power stage for three-phase motors.

More details available @ https://www.st.com/en/evaluation-tools/steval-ctm009v1.html

  • Industrial PLC evaluation board with HMI interface

The STEVAL-PLC001V1 evaluation board targets compact programmable logic controller (PLC) applications in the factory automation domain. It features a powerful human machine interface (HMI) thanks to the 3.5” TFT touchscreen mounted on the PCB, which eases interaction with the tool.

More details available @ https://www.st.com/en/evaluation-tools/steval-plc001v1.html

 

STM32 ecosystem & graphics

Artificial Intelligence Ecosystem:

  • NanoEdge AI Studio: Automated Machine Learning (ML) tool for STM32 Developers

NanoEdge™ AI Studio (NanoEdgeAIStudio) is a Machine Learning (ML) tool that allows developers to create an optimal ML library for their project, based on a minimal amount of data.

Predictive Maintenance with NanoEdge AI
This demo shows how to detect abnormal behavior of the motor in relation to the dynamically learned model, based on current sensing. It calculates the anomaly based on a pre-trained AI model created with NanoEdge AI Studio. Different motor speeds can be dynamically learned by the operator using the potentiometer speed selector. The rotating belt can be altered by the operator using the knobs, altering the motor rotation and changing the motor current drained. The display shows the current status, motor speed and behavior.

  • STM32Cube.AI: STM32Cube.AI software tool is part of the STM32Cube ecosystem and supports models from the main AI training frameworks.

If you already have AI design skills and have created your own ANN models, STM32Cube.AI comes with many example applications. You will find debugging tools, and pre-integrated libraries to get you started quickly.

Automatic reading of mechanical water meter with AI : the demo shows the ability to read the numbers of a water meter and the transformation into digital information through an AI system composed of STM32H747I-DISCO and B-CAMS-OMV

Security for embedded systems:

  • STM32Trust: a security framework to protect embedded systems

Advanced graphics ecosystem:

  • STM32 Graphical User Interface (GUI) :

Creating a good GUI requires skills and expertise. It involves many building blocks, starting with the selection and sourcing of the right display and casing, the art-creation of menus and screens, the programming of the art-design into a user interface and the electronic development.

ST provides state-of-the-art MPUs and MCUs, combined with the tools and the support you need every step of the way, to ensure you bring your GUI project to success.

STM32 GUI developer portfolio and kits: 

  • X-CUBE-LocalVUI
    Local voice user interface software expansion

X-CUBE-LocalVUI implements cloudless local voice recognition user interfaces based on audio capture, and speech recognition. It integrates the Sensory TrulyHandsfree™ (THF) and TrulyNatural™ (TNL) software, and VoiceHub generated vocabulary examples. It also integrates the Picovoice Porcupine and Rhino software, and the Picovoice console generated vocabulary example. The audio capture is based on STM32 peripherals and middleware. It shows how to capture audio from the board microphone through SAI.



STM32H747I-DISCO Discovery kit

  • NFC / RFID tags & readers


ST25 series lets you design an advanced, integrated NFC Reader+Tag solution.
Watch this video to learn more.

IoT & Connectivity

  • BLE based Smart Plug 

 

The STDES-BLUEPLUG2 is a reference design for home-automation and Internet of Things (IoT) applications. The on-board BLUENRG-M2SP is compliant with Bluetooth® Low Energy (BLE) specification 5.2 to allow secure communication of metering data from specific electrical loads to a smartphone with BLE support. It supports multiple roles simultaneously and can act at the same time as Bluetooth smart master and slave device. The device current consumption on AC mains is 3 to 7 mA.  The device acts as a BLE peripheral device which can be connected to any smart device using the Android ST BLE PLUG app (available for free download on Google Play) to control and monitor the load and its energy settings. The app features load ON/OFF turning, scheduling, dimming and metering settings.


The STDES-BLUEPLUG2 embeds an STPM32 metering chip for high accuracy measurement of power and energy in power line systems using shunt current sensors, a three-terminal TRIAC which controls the current through AC switching for various electrical system applications, and a non-isolated buck converter supply based on the VIPER06XS. This type of supply is ideal for the applications (like ST BLE PLUG) where a large amount of current is not needed and a small form factor is required.

More details available @ https://www.st.com/en/evaluation-tools/stdes-blueplug2.html

  • BLE Mesh lighting demo

Users can connect Bluetooth® Low Energy nodes to a smartphone via Bluetooth® Low Energy, through a suitable Android™ or iOS™ application, to set the HSL values and send the data to the lighting hardware using the Bluetooth® Low Energy mesh lighting model.

More details available @
https://www.st.com/en/embedded-software/fp-lit-blemesh1.html
https://www.st.com/en/embedded-software/stblemesh.html

  • Sub-1GHz and inertial sensors expansion board for STM32 MPU

X-LINUX-IOT01E/A is an STM32 MPU OpenSTLinux software expansion package, which runs on the Arm® Cortex® A7-based core of the STM32MP1 microprocessor.
In the STM32MP157F-DK2 discovery kit, it demonstrates the SPIRIT1 and LSM6DSOX-based applications, using the X-STM32MP-IOT01A hardware expansion board.

More details available @ https://www.st.com/en/embedded-software/x-linux-iot01e-a.html

  • Multi-sensor platform for STM32MP1 MPU

The X-STM32MP-IOT01A is an STM32 MPU expansion board with the SPSGRF-915 SPIRIT1 RF module for Sub-1 GHz RF communication with sensor, for IoT applications.
The X-STM32MP-IOT01A interfaces with the STM32MP1 microcontroller via GPIO connector pins, using SPI, I²C, GPIO connections for the SPSGRF-915, iNEMO inertial module, keys, and LEDs. It is compatible with the STM32MP157F-DK2 and Raspberry Pi’s GPIO connector layout.

More details available @
https://www.st.com/en/evaluation-tools/x-stm32mp-iot01a.html
https://www.st.com/en/evaluation-tools/stm32mp157f-dk2.html

  • Global Navigation System (GNSS) for STM32 MCU and MPU platforms

The X-NUCLEO-GNSS1A1 expansion board is based on the Teseo-LIV3F tiny GNSS module. It is an affordable GNSS module, embedding a Teseo III single-die standalone positioning receiver IC, usable in different configurations in your STM32 Nucleo project. The Teseo-LIV3F is a compact (9.7 x 10.1 mm) module that provides superior accuracy thanks to the on-board 26 MHz temperature compensated crystal oscillator (TCXO) and a reduced time-to-first fix (TTFF) with its dedicated 32 KHz real-time clock (RTC) oscillator.

The Teseo-LIV3F module runs the GNSS firmware (X-CUBE-GNSS1) to perform all GNSS operations including acquisition, tracking, navigation and data output without external memory support. The X-NUCLEO-GNSS1A1 expansion board is compatible with the Arduino™ UNO R3 connector and the ST morpho connector, so it can be connected to the STM32 Nucleo development board and stacked with additional STM32 Nucleo expansion boards.

More details available @ https://www.st.com/en/ecosystems/x-nucleo-gnss1a1.html

For your health and safety, we are firmly committed to implementing all the necessary measures to comply with local regulations.


For questions related to registration, do not hesitate to write to us at : nidhi-sehgal.kaul@st.com