Webinar - New Bluetooth modules based on BlueNRG QFN package

Join us for our webinar on the new BlueNRG Bluetooth® low energy modules and their development ecosystem

 

Tuesday, September 17th 2019, 3 PM CET

 

Discover and understand our new BLE module portfolio and development ecosystem

In this webinar you will learn about STMicroelectronics' new Bluetooth® Low Energy modules portfolio and their development ecosystem. 

Equipped with an on-board antenna, crystal oscillator and RF balun, ST’s BLE modules offer a proven, robust solution that ensures a quick time-to-market. They come with the embedded Bluetooth stack to provide a certified Bluetooth Qualification Expert (BQE) solution that is also fully RED, IC and FCC approved, thus ensuring rapid integration into the final application and providing an easy-to-use solution.

Our Bluetooth Low Energy modules are supported by an extensive set of evaluation boards, software development kits, application notes and design guidelines – thus facilitating the adoption of Bluetooth wireless connectivity technology into a wide variety of application segments

Agenda

  • BlueNRG family roadmap update.
  • Benefits of our BLE modules: Hardware integration and certification.
  • Why new modules and for which application?
  • Description of new BlueNRG-M0 BLE master/slave network processor module and overview of development tools
  • Description of new BlueNRG-M2 BLE master/slave network processor module and overview of development tool

There will be a live Q&A session at the end of the webinar where ST’s experienced engineers will be available to answer your questions.

Product information

Our very-low-power BlueNRG-M0 master/slave network processor module for Bluetooth® Low Energy v4.2 offers a proven, robust solution that ensures a quick time-to-market.
 

Registration information

There is no charge to participate in this event, but you must register through my.st.com.

 

If you have a myST accountRegister Now

 

If you do not have a myST accountCreate An Account

 

 

Speaker

Laurent Louazon has worked for more than 20 years on wireless communication systems including 2G/3G/4G cellular, Bluetooth and Wi-Fi.His main focus is to support customers developing applications based on the Bluetooth Low Energy technology.
With more than 15 years on wireless communication systems including 2G/3G cellular, Bluetooth and Wi-Fi, Dominique Follezour is a valued member of ST´s wireless application team. His main focus is to support customers developing applications based on the Bluetooth Low Energy technology.
A valued member of ST´s wireless application team, Sébastien Denoual has worked for more than 15 years on wireless communication and embedded system (multimedia application). Sebastien's main focus is to support customers developing applications based on Bluetooth Low Energy technology

今後のイベント

SENSOR+TEST 2021 16 Apr - 06 May, 2021
PCIM 2021 16 Apr - 07 May, 2021