RADECS 2016

Congress Centre Bremen
September 19th to 23rd, 2016
Website: Click here
Visit us at booth #37
The 2016 Radiation Effects Conference features a technical program consisting of technical sessions each with contributed papers describing the latest observations in radiation effects. An industrial exhibit will complete the event.
ST's Space Product Team and radiation experts will present ST's latest additions to its portfolio of Space products, including:
Rad-Hard analog and power products with best-in-class radiation and electrical performance
- New generation of Rad-Hard Power Schottky diodes & rectifiers
- Expanding portfolio of 100 krad ELDRS bipolar transistors
- Expanding series of Rad-Hard enhanced LVDS solutions
- Expanding Rad-Hard Op amp portfolio
- "Hot" new announcements of its Rad-Hard 16-bit ENOD D/A converter
- New generation Rad-Hard voltage regulator
- New best-in-class series of Rad-Hard Gate Drivers
- .... and more to come
ST high density ASIC & ASSP radiation hardened design platforms
- ST's 65 nm high density mixed signal technology for Rad-Hard ASIC & ASSP
- Technology Roadmap
ST has a broad offer to support designs in 28nm FD-SOI with a variety of key design block available to designers.
Details on the radiation test results of some these products will also be presented at the technical conference