STM32G4 mixed-signal MCU hands-on workshop series
![]() | |
Join our experts for a free hands-on workshop and learn what makes the new STM32G4 mixed-signal MCU ideal for todays advanced control and measurement applications.
With a rich set of analog peripherals, mathematical accelerators and high resolution timers, the STM32G4 is a great fit for applications including three-phase brushless motor control, instrumentation and digital switch-mode power supplies.
This one-day hands-on workshop will introduce embedded engineers to the new features of the STM32G4 through hands-on exercises, using the STM32G474 Discovery board. The board features the STM32G474RET6 MCU based on an Arm® Cortex®-M4 core operating up to 170 MHz with 512 Kbytes of Flash memory, 128 Kbytes of SRAM in a LQFP64 package along with several application circuits including a digital power buck-boost converter and RGB power LED.
Application engineers will be available on-site to provide technical support and answer your questions during the session.
Who should attend?
This workshop was developed for embedded engineers working with microcontrollers for digital control applications.
You will learn:
- The new features and peripherals of the STM32G4 microcontroller series
- How to get started with the STM32G474 Discovery kit (B-G474E-DPOW1), STM32CubeMX and Keil MDK
- How to configure and use the new features of the STM32G4 through hands-on exercises
Registration information
There is no charge to participate in this event, but it is necessary to register through my.st.com.
Workshop Agenda*
8:00 – 9:00 |
|
9:00 – 12:00 |
|
12:00 – 1:00 |
|
1:00 – 3:00 |
|
*The above agenda applies to the full-day workshop sessions. A shorter version of the workshop will be held at ST Developers Conference 2019, at ST Technology Tour events, and at Arm TechCon. Click "Learn more" in the table below for details on how to register for these events.
Prerequisites
You will need a laptop with a Type A USB port and administrator rights running Windows 7 or later, or a MacBook running Windows (Parallels, VM Fusion, etc.), with a minimum 2 GHz processor, 4 GBs of RAM and 10 GBs of free disk space. For laptop with only USB Type C ports, please bring a Type A (Female) to Type C (Male) adapter. ST will provide the development kit. You must stay for the training session to receive the free kit.
Workshop Dates and Locations (subject to change)
City | Date | Location | Status |
Chicago (Schaumburg), IL | Sep 10, 2019 | STMicroelectronics 1st Floor Lobby Meeting Room (the forum) 200 N Martingale Rd Schaumburg, IL 60173 847-585-3000 | Closed |
Santa Clara, CA | Sep 12, 2019 | 3-hour workshop session at ST Developers Conference 2019 Learn more | Closed |
Vancouver, BC | Sep 24, 2019 | 3-hour workshop session at ST Technology Tour 2019 - Vancouver Learn more | Closed |
São Paulo, Brazil | Sep 25, 2019 | São Paulo Center Avenida Lineu de Paula Machado, 1088/1100 Cidade Jardim – São Paulo, SP 05601-001 +55 11 2142-3600 | Closed |
Dallas, TX | Sep 26, 2019 | Renaissance Dallas Richardson Hotel 900 E Lookout Drive Richardson, TX 75082 972-367-2000 | Closed |
Houston, TX | Oct 1, 2019 | Courtyard Houston Katy Mills 25402 Katy Mills Parkway Katy, TX 77494 281-665-3189 | Closed |
Philadelphia, PA | Oct 3, 2019 | The Desmond Hotel Malvern 1 Liberty Blvd Malvern, PA 19355 800-575-1776 | Closed |
Milwaukee, WI | Oct 8, 2019 | Embassy Suites by Hilton Milwaukee Brookfield 1200 South Moorland Road Brookfield, Wisconsin 53005 262-782-2900 | Closed |
Waterloo, ON | Oct 8, 2019 | Delta Hotels Waterloo 110 Erb Street West Waterloo, Ontario Canada N2L 0C6 519-514-0404 | Closed |
San Jose, CA | Oct 9, 2019 | 3-hour workshop session at Arm TechCon 2019 Learn more | Closed |
Toronto, ON | Oct 10, 2019 | Toronto Airport Marriott Hotel 901 Dixon Road Toronto, ON Canada M9W 1J5 416-674-9400 | Closed |
Orlando, FL | Oct 22, 2019 | Hilton Garden Inn Orlando at SeaWorld 6850 Westwood Blvd. Orlando, FL 32821 407-354-1500 | Closed |
Pittsburgh, PA | Oct 22, 2019 | The RLA Learning and Conference Center 850 Cranberry Woods Drive Cranberry Township, PA 16066 724-741-1000 | Closed |
Charlotte, NC | Oct 24, 2019 | Hilton Charlotte University Place 8629 JM Keynes Dr Charlotte, NC 28262 704-547-7444 | Closed |
Indianapolis, IN | Oct 24, 2019 | Marriott Indianapolis North 3645 River Crossing Pkwy Indianapolis, IN 46240 317-705-0000 | Closed |
Minneapolis, MN | Oct 24, 2019 | 3-hour workshop session at ST Technology Tour 2019 - Minneapolis Learn more | Closed |
Montreal, QC | Oct 29, 2019 | Hotel Ruby Foo 7655 Decarie Blvd Montreal, QC Canada H4P 2H2 514-731-7701 | Closed |
Orange County, CA | Oct 29, 2019 | DoubleTree by Hilton Irvine 90 Pacifica Irvine, CA 92618 949-471-8605 | Closed |
Boston, MA | Nov 5, 2019 | 3-hour workshop session at ST Technology Tour 2019 - Boston Learn more | Open |
NOTE: All locations subject to change.