Find a partner

Products and Services
Total results: 5 partners
Showing partners per page

AWS

Amazon Web Service (AWS) IoT is a managed cloud platform that lets connected devices easily and securely interact with cloud applications and other devices. AWS IoT can support billions of devices and trillions of messages, and can process and route those messages to AWS endpoints and to other devices reliably and securely. With AWS IoT, your applications can keep track of and communicate with all your devices, all the time, even when they aren’t connected.

STMicroelectronics is Standard Technology Partner in the AWS Partner Network (APN).
 
(#STSAFE-A) (#STSAFE-J) (#STSAFE-TPM) (#STSECURE)
 

Microsoft

Transform your business with Internet of Things.
Build things : IoT begins with your things. Build with your things, from adding sensors to creating smart devices, to start your IoT solution.
Control your things : Deploy IoT solutions that control, monitor, and manage your things, allowing you to capture real-time data. 
Analyze data : Take the data you collect and apply advanced analytics to uncover new business insights. 
Act on insights : Transform insights into action through powerful applications—creating new revenue and business opportunities.

(#STSAFE-A) (#STSAFE-J) (#STSAFE-TPM) (#STSECURE)

Mocana

Mocana’s end-to-end cybersecurity system protects millions of industrial control systems and smart connected devices that comprise the Internet of Things across all sectors.

"Mocana" means to set free, and our mission is to protect countries, cities, and families by enabling devices of every kind to be trustworthy and run securely and freely. Mocana was founded in 2002 to help protect military aircraft, vehicles, and devices. Our security software protects devices by using cryptography designed to run on microcontrollers and embedded devices. Today, we serve both the defense and commercial sectors.

Mocana is now running on every type of device you can imagine: fighter jets, helicopters, tanks, commercial aircraft, industrial automation and controls, thermostats, surveillance cameras, network gateways, set top boxes, medical devices, and much more. In fact, we now protect more than 100 million devices.

200 of the largest industrial manufacturing, aerospace, defense, utilities, energy, and transportation companies trust Mocana to harden their mission-critical devices and secure IoT communications using Mocana TrustPoint, our embedded IoT endpoint software, and Mocana TrustCenter, our automated security services platform. Our solutions enable our customers to secure their manufacturing supply chain.

Together, let's secure the Internet of Things from the inside out.

(#STSAFE-A) (#STSAFE-J) (#STSAFE-TPM) (#STSECURE)

Prove & Run

Prove & Run was created with the idea that large-scale deployments of connected devices is an attractive target for remote cyberattacks and that the solutions used in the mobile industry are not sufficient to answer to the challenge. Prove & Run answers to the cybersecurity requirements of the device OEMs at all steps of their product life-cycle by providing: 

• Security consulting services such as performing security analysis, defining security architecture and security requirements

• Solutions to secure-by-design their devices

When designing connected devices, security engineers can rely on three pillars:

1. Secure Elements

2. Trusted Execution Environments (TEE) or secure OSs

3. Hardware- or software-based hypervisors

In order to resist to sophisticated remote attacks, Prove & Run has designed TEEs and hypervisors that are highly resistant against hackers and as close as possible to zero bugs and that can be used in complement to the Secure Elements to secure by-design the OEM's devices. 

(#STM32MPU) (#STM32MP1) (#STSAFE-A) (#STSAFE-J) (#STSAFE-TPM) (#STSECURE)

wolfSSL

The wolfSSL embedded SSL library is a lightweight, portable, C-language-based SSL/TLS library targeted at IoT, embedded, and RTOS environments primarily because of its size, speed, and feature set. It works seamlessly in desktop, enterprise, and cloud environments as well. wolfSSL supports industry standards up to the current TLS 1.3 and DTLS 1.2, is up to 20 times smaller than OpenSSL, offers a simple API, an OpenSSL compatibility layer, OCSP and CRL support, is backed by the robust wolfCrypt cryptography library, and much more.

The CMVP has issued FIPS 140-2 Certificates #3389 and #2425 for the wolfCrypt Module developed by wolfSSL Inc.  For more information, see our FIPS FAQ.

(#STSAFE-A) (#STSAFE-J) (#STSAFE-TPM) (#STSECURE)