Find a partner

Products and Services
トレーニング: 283 検索結果
Showing パートナー

Electric Imp

Electric Imp offers an innovative and powerful Internet of Things (IoT) platform that securely connects devices with advanced cloud computing resources. Our unique solution — featuring fully integrated hardware, OS, security, APIs and cloud services — dramatically decreases cost and time to market while increasing security, scalability and flexibility.  The Electric Imp platform enables innovative commercial and industrial applications and empowers manufacturers to manage and quickly scale their connected products and services to millions of users.

Elektrobit

Elektrobit offers a complete portfolio of products that adds a direct value in terms of reduced initial development costs. It also creates even higher values long term:

  • Component based AUTOSAR tools based on a proven methodology and renowned system development tools chain increases productivity.
  • Leveraging on standardized products supporting model-based development improves quality and makes complexity manageable.
  • Full access to embedded source code and a tools chain built on industry-leading open source projects enabling transparency and flexibility.
  • Supports agile software development based on re-use of software and a tools chain that enables distributed development in global teams.

 

Elprotronic

Elprotronic Inc. offers flash programming solutions for a wide variety of embedded MCUs. We deliver quality and reliable production programmers, that provide top performance, and software flexibility for both low and high volume production. We provide programmers with up to 1MB/s data transfer and built-in galvanic isolation, programmable communication clock up to 20 MHz, real-time current measurement, and both USB and Ethernet connectivity. Our software supports both Linux and Windows(TM)  ME, 2000, XP, 7, 8, 10.  In addition, we can offer our customers customized solutions for more challenging production and programming requirements, dependent on the requirements of the hardware. For all our clients, we pride ourselves on timely and helpful customer service, and constantly improving our products based on user feedback.

EMAC

EMAC provides Hardware & Software Engineering Design Services having developed strong expertise on Industrial IoT 
We also offer a number of Embedded Off-The-Shelf Hardware Products.
These Hardware Products can be loaded with a variety of Off-The-Shelf Software Products including Linux and Windows. 
EMAC has in-house manufacturing capability, allowing us to manufacture the Hardware that we design.

Embedded Office

Embedded Office is founded in 2003 in Germany with focus on safety consulting. The engineers are certified experts in embedded software development for safety critical systems. With the unique "Safety Mentoring" the success of software approvals for usage in systems according to IEC 61508, ISO 262626, IEC 62304 or DO-178C is guaranteed. Provided software components and complete platform integrations are completing the service to minimize efforts for new projects in safety and security.

On request, the service called "Safety Mentoring" will provide your project with a development partner who works proactively in your project, and supports you with the introduction of development processes through workshops, training and suggestions.

(#FuSa)

Embedded Partners

Embedded Partners offers professional software development services. We bring long and wide experience in development software systems and projects in a verity of disciplines. Our core competence is real time embedded systems and over the years we development also application systems in the surrounding environment of those Real-Time systems, such as management, control, and configuration.
We are official implementer partners of TouchGFX, a leading supplier of software framework for development of graphical user interface (GUI) to low-resource hardware. We have hands-on experience working with TouchGFX framework that allow us to offer to our customers a fast and secure path to fulfill their GUI and other embedded graphical needs while allow them to concentrate in their core system development.

We have experience in data, video & VOIP communication, microcontrollers and integrate open source solutions. We worked with a large variety of operating systems, controllers of STMicrocontrollers, STMicrocontrollers development tools such as System Workbench, CubeMXetc.  Segger debug tools such as Ozone, SystemView, etc. and various development environments  such as Eclipse, IAR Embedded Workbench, and more.

Our services refer to both companies that need an answer to a fast development needs, might be a short project or ongoing activity, as well as companies which have development needs in their surrounding area of expertise.

We offer long and ongoing availability and support, fast response and rapid domination of the customer needs and development environment. Along with the professional experience in software development we bring also a wide system view, business view and marketing knowledge that can serve as an added value to the development expertise.

To customers need we can provide turn-key solutions that includes, in addition to software development, hardware and/or mechanical development. We can bring our own partners or team up with the customer own development team or other third-party development providers

Embedded Wizard

TARA Systems is a technology-driven software company providing components and services for embedded systems in the field of consumer electronic, industrial, medical, automotive, and mobile devices. We focus on reliable solutions for Graphical User Interface tools and developments as well as digital TV reception. More than 25 years of experience in these domains enable us to offer our customers high quality innovative products. These allow them to differentiate from competitors and appeal to the users.


With Embedded Wizard, TARA Systems released its fourth generation of GUI development tools, driven by the idea to provide a comfortable workflow for embedded systems, which has been known only in PC development until now. GUIs created with Embedded Wizard have been deployed on more than 100 millions devices worldwide.


(#STPMIC1) (#STM32MPU) (#STM32MP1)

 

Emcraft Systems

Emcraft Systems designs, manufactures and sells Arm Cortex-M System-On-Modules and software distributions based on the following ST devices: STM32MP1, STM32F4, STM32F7 and STM32H7.

On the software side, we provide production-ready, self-maintained Linux Board Support Packages (BSPs): STM32F746G Discovery BSP, STM32F769I Discovery BSP and STM32F4 Discovery BSP. (#STM32MPU) (#STM32MP1)

emotas

emotas GmbH is an embedded software development company located in Merseburg, Germany.
The main focus of the product portfolio lies on CAN, J1939, CANopen/CANopen FD, EnergyBus and EtherCAT protocol stacks and tools. By providing highest quality and best service we will be our customer’s reliable partner. Not only do we develop software products, also tailored embedded software solutions according to customers’ requirements are part of our offered services.
The range of service covers consulting for developments and integrations as well as software maintenance and CANopen and EtherCAT trainings. By taking part in work groups and standardizing boards of CiA and ETG we are always on top of the developments and so are emotas' products.

(#STM32MPU) (#STM32MP1)  

eMoticom

eMoticom established in 2016 develops and manufactures electronics for use in the automotive field and for the conversion and storage of energy.

Despite being a young company, eMoticom’s founders and engineers have decades of experience and know-how in endothermic engine controls, specializing in products for motorbikes (both for competitions and for OEM) for several world-renowned motorcycle companies.

eMoticom does not only provide electronic products but also offers the customers research and development services so as to define and create ad-hoc products most suited to their requirements with special attention to the integration of innovative solutions.

eMoticom’s engineers also boast of an in-depth knowledge of energy conversion systems for power supply inverters as well as electric traction and energy storage systems for electrical vehicles which, in combination with the know-how of classic traction vehicles, completes their knowledge and gives them the ability to develop hybrid products.

For the development and manufacture of its products, eMoticom avails itself of a network of engineers with a vast experience in both electronical and mechanical fields which allows the company to create technologically innovative products with particular attention to quality whilst maintaining competitive prices and optimal time to market.

emtrion

emtrion GmbH from Karlsruhe has been supporting customers for more than 20 years as a system integrator for embedded complete solutions at all levels of the development process. 

The product spectrum ranges from hardware and software design over application development and housing construction to series production and assembly, Made in Germany.

Solutions for the Internet of Things (IoT), virtualization on multicore CPUs, security and safety are just as much a part of the offering as are customer-specific solutions and industrial real-time communication. (#STM32MPU) (#STM32MP1) (#STPMIC1)  

 

ENEA

Enea develops the software foundation for the connected society. We provide solutions for mobile network traffic management, network virtualization, network traffic classification, embedded operating systems, and professional services. 

Solution vendors, systems integrators, and service providers rely on Enea when creating new world leading networking products and services. More than 3 billion people around the globe already depend on Enea technologies in their daily lives. 

(#STPMIC1) (#STM32MPU) (#STM32MP1)

Engicam

Engicam is an Italian company based at Firenze in Scandicci, entirely managed by the owners. Engicam was founded in 2004 with the aim of providing design services of electronic systems with high content of technology, relying on a long experience in electronic design.
Considering customers as his partners, allowed Engicam to successful develop collaborations with the key OEM’s in consumer, automotive, marine and railway fields, and with small and medium companies operating in niches of industrial market.

The continued investment allows Engicam to provide and develop more and more powerful and efficient platforms.

The philosophy of Engicam is to assist its customers throughout the development process towards the final system. Engicam provides both high-level hardware and software support from product development to mass production. (#STM32MPU) (#STM32MP1)

ESCRYPT

ESCRYPT – Embedded Security is the leading system provider for embedded IT security. At five German locations and in branch offices in the United Kingdom, Sweden, the United States, Canada, India, China, Korea, and Japan, our experts are concentrating on current data security issues, such as: Automotive Security, M2M communication, IT security in the Internet of Things, Securing e-business models.

 

eSoftThings

eSoftThings specializes in designing, developing and deploying IoT Platforms as well as Automotive and Audio solutions. 

We have developed our proprietary secure end-to end IoT platform. Initially deployed in the utility space, but active in other verticals. 

We develop optimal solutions for Advanced Driver Assistance Systems (ADAS) and Autonomous Vehicles (AV). 

We have unique expertise in computer vision algorithms, mathematical models for deep machine learning, data set conditioning and cloud infrastructures. 

Our Audio capabilities include full electronics design and development for military grade headsets, advanced consumer telephony and smart speaker solutions. 

We specialize in connectivity, power optimization, HMI (Human Machine Interface), and acoustic design and tuning. 

ETAS

​ETAS provides innovative solutions for the development of embedded systems for the automotive industry and other sectors of the embedded industry. As a systems provider, ETAS supplies a multifaceted portfolio that covers the range from integrated tools and tool solutions to engineering services, consulting, training, and support. Security solutions in the area of embedded systems are offered by the ETAS subsidiary ESCRYPT. Established in 1994, ETAS GmbH is a 100-percent subsidiary of the Bosch Group, with international subsidiaries and sales offices in Europe, North and South America, and Asia.

 

Evatronix

Evatronix is an engineering company based in Bielsko-Biala, Poland established in 1991. Our mission is enabling our customers to bring innovative electronic products to the market.

We realize it through:

  • comprehensive offering of outsourced electronic product development and focused engineering services, covering the whole design flow from product specification, product architecture, embedded software and hardware development, verification and validation
  • product prototyping and supply chain management in low volume production,
  • sales and deployment of modern design tools for electronic and mechanical engineers along with consulting and training in this domain (our VAR division, only in the Polish market).

Exosite

Exosite is a mix of IoT-obsessed experts who provide enterprise IoT solutions, powered by our platform, to accelerate customer success. Exosite has been connecting things to the Internet for years and have helped customers transform from traditional into connected to optimize cost, eclipse the competition, and create new revenue.

Exosite is recognized as an IoT leader

  • Cool vendor in the internet of things by Gartner 2017
  • Top 11 most significant IoT platform providers by FORRESTER

EXPERTiS

EXPERTiS is an engineering design services company with more than 20 years of experience in electronic and embedded product development.

Over 200 products for the consumer, industrial, automotive and telecommunications markets are behind our staff expertise.

We can provide a one stop full product development that covers the entire cycle from concept to production. Our areas of expertise covers embedded internet devices, automotive CAN enabled ECU and EMU design, USB enabled devices, ultra low power design for instrumentation, telemetry and wireless.

Express Logic

Express Logic headquartered in San Diego, California provides the popular ThreadX®, a pre-certified, Industrial-grade RTOS, along with a suite of advanced middleware for embedded applications, and the X-Ware Platform optimized to help IOT developers get to market faster. Express Logic has achieved over 5.4 billion deployments of ThreadX since its founding by William E. Lamie in 1996. Express Logic values simplicity and making embedded IoT development as easy as possible. Express Logic believes in making the fastest, smallest, most secure and highest quality solutions to help customers achieve the same in their products.

(#FuSa)