Brushless DC Motor Parameter Characterization
Overview
Title: BLDC Motor Parameter Characterization
Duration: 23 minutes
Summary
This video will present proven techniques for measuring the essential BLDC motor parameters using readily available electronics laboratory equipment. A discussion of the measurement challenges that are presented when characterizing low resistance and low inductance motors is also presented. Several different techniques are presented, conducting the tests on both a typical and a more challenging motor.