STM32WB dual-core wireless MCU webinar

STM32WB Powers Next-Generation IoT Devices with Bluetooth® 5.0 & 802.15.4



Explore the new STM32WB, the first and only dual-core Cortex-M4 and Cortex-M0+ wireless MCU on the market certified for Bluetooth® Low Energy 5.0 and IEEE 802.15.4.

Miss the webinar? You can view the 1-hour recording to learn about the STM32WB, a wireless microcontroller that combines Bluetooth® 5.0, OpenThread, and ZigBee® 3.0 connectivity with ultra-low-power performance.

You will learn how to develop with the STM32WB using the rich STM32Cube ecosystem, which includes all the tools needed to easily develop Bluetooth, Thread and proprietary applications while utilizing STM32CubeMX for peripheral configuration, middleware additions, and connectivity libraries. By the end of the video, you will have a solid knowledge base to start developing using the P-NUCLEO-WB55 development pack.

You will learn

  • The key features and peripherals embedded in the STM32WB
  • How to get started with the STM32CubeMX 5.0 graphical software configuration and code generation tool
  • To use STM32CubeProgrammer to program the STM32WB and STM32CubeMonitorRF for rapid Bluetooth prototyping
  • Where to find pre-built examples, applications, and code for reuse

Speakers

Alec Bath is the Eastern Region Applications Manager for Microcontrollers and is celebrating his 20th year with ST. Alec has supported ARM-based microcontroller families, the STR7 & STR9, and now the highly successful STM32 family ever since. Prior to ST, Alec worked as a hardware design engineer at Motorola for analog cellphones and automotive body electronics modules.  
Colin Ramrattan has been with ST Microelectronics since 2012 and is a Product Marketing Engineer with the microcontroller product marketing team for the Americas. Colin has held positions in both the analog sensors and connectivity organization previous to microcontrollers. Prior to ST Microelectronics Colin was a user interface module designer at Blackberry in Waterloo, Canada.  

 

About the STM32WB Wireless Series

The STM32WB series is a dual-core, multi-protocol and ultra-low-power 2.4 GHz MCU system-on-chip. It supports Bluetooth™ 5 as well as IEEE 802.15.4 communication protocols (in Single and Concurrent modes) covering a wide spectrum of IoT application needs.

Based on ST’s best-in-class, ultra-low-power STM32L4 MCU, the STM32WB series reduces development time and BOM cost, extends application battery life and inspires innovation thanks to its rich and flexible peripheral set.

The STM32WB series is designed to fit industrial, healthcare and consumer applications.

活动预告

2021年STM32中国峰会 08 Mar - 29 Apr, 2021
PCIM 2021 16 Apr - 07 May, 2021
SENSOR+TEST 2021 16 Apr - 06 May, 2021