Embedded Vision Summit 2022
Embedded Vision Summit 2022
May 17 19, 2022
America, Santa Clara, CA
Registration and detailed Agenda
ST will join industrial leaders for discussion on Join ST and Industry leaders to discover all the newest technologies contributing to Embedded Vision. From AR, VR, Machine Learning, Contactless High Gigabyte data transfer AND Image Sensors, ST has innovative new technologies you won’t want to miss.
- Join Armita Abadian, Product Marketing for Imaging, at 4:15 on Tuesday May 17 for a discussion on How Ultra Low Power (ULP) drivers open new potential applications for Time of Flight (ToF) sensors.
- Abstract: The ULP drivers allow the ToF sensors to function as proximity detectors. The settings and flow have been specially designed to reduce the power consumption. Using the proposed configuration, the current consumption can be reduced down to 55 μA at 1 Hz ranging frequency with a 2V8 power supply. All the processing is fully embedded in the sensor firmware. Instead of outputting default data like distance, signal, SPAD nb, etc., the implemented mechanism raises an interrupt to the host when a target is detected in the field-of-view.