STSPIN32 Motor Drivers Introduction Webinar
![]() | Explore how STSPIN32 brings intelligence in 3phase BLDC motor control, allowing the convergence of analog and digital worlds - 1 hour webinarThis webinar was broadcasted Thursday, August 6th 2020 | 11:30 am IST (UTC+05:30) |
ST, a pioneer in the field of motion control, offers a wide spectrum of drivers to best match an extensive range of possible combinations of voltages, currents, innovative features and motor types.
STSPIN motor drivers embed all the functions needed to drive the most diffused motors efficiently and with the highest accuracy, while ensuring scalability, robustness and reliability.
STSPIN32 family consists of low voltage and high voltage intelligent drivers made by a Cortex-M0TM STM32 and an advanced 3-phase gate driver. These devices span from full featured and self-supplied drivers, with embedded current sensing, suitable for battery operated applications, to very rugged 600V gate drivers with embedded fail-safe protections for off-line applications. In both cases, the embedded MCU gives the freedom to configure the device with the motion control algorithm which best fits the end application targets.
During this 1-hour session, you will get an overview of both low voltage and high voltage STSPIN32 devices and will learn about related evaluation tools and ecosystem. Some practical application examples on vacuum cleaner and fridge compressor will be introduced as well.
There will be a live Q&A session at the end of the webinar where ST’s experienced engineers will be available to answer your questions.
Agenda
- Introduction and overview of STSPIN32 family
- STSPIN32F0 Low Voltage & High Voltage series deep dive
- Hardware and Firmware ecosystem for fast evaluation and prototyping
- Practical examples
Speakers
![]() | Satish Pawar Senior Manager Technical Marketing - Power Discrete & Sub Analog Experience in Semiconductor Industries more than 25 years, He is working with ST from last 13th year as Technical Marketer, His main filed of interest as dedicated market development in field of Motor Control & Home Appliances taking care of IGBT, IPM, Mosfet and Power Module. Satish helps motor control engineers find best solutions for their applications. | |
![]() | Yew-Kuan LEE Technical Marketing Manager YK LEE has more than 25 years of Technical Marketing experience in Motor Control and Power Discrete. He provides best Motor Control solutions such as Three Phase Brushless DC Motor, Stepper Motor and Brush DC Motor to customers. With optimum performance, high reliability and most competitive pricing in mind, the solutions were well received and adapted by his customers. Furthermore, he is in charge of other key products :- AC-DC, DC-DC Power Management, Industrial Drivers, etc. | |
![]() | Siddharth GHOSH Sr. Manager - Technical Marketing for Power Discrete and Sub Analog Group Siddharth holds a Master Degree in Power Electronics from Indian Institute of Technology ( IIT Delhi ). He joined ST Microelectronics (ST) in 2011 as Product Marketing Manager. He is presently working as Sr. Manager - Technical Marketing for Power Discrete & Sub Analog Group (PDSA) with focus on key products :- AC-DC Power Supply, Offline PWM Controllers, DC-DC Power Management , Motor Drivers etc. |