意法半导体合作伙伴计划增强了意法半导体广泛的产品组合的生态系统,帮助他们减少开发工作并加速产品上市时间。
意法半导体合作伙伴计划的成员提供广泛的产品和服务,涵盖软件开发工具、硬件开发工具、嵌入式软件、组件和模块、培训、工程服务和云等领域。
法律免责声明
除了本网站所载的使用条款、意法半导体销售条款和条件以及隐私政策,以下条款和条件适用于所有意法半导体合作伙伴计划。
尽管意法半导体已经尝试在网站上提供准确的信息,但意法半导体对信息的准确性不承担任何责任。意法半导体在本网站提供的所有信息均按“原样”提供,并包括所有错误,且无任何形式的保证,无论是明示的、默示的还是法定的。意法半导体可能随时更改或停止其合作伙伴计划或其产品或服务,恕不另行通知。对于非意法半导体产品或服务的任何提述仅供参考,不构成意法半导体的认可。在本网站上使用“合作伙伴”一词不表示或暗示意法半导体与任何其他公司之间存在任何合作伙伴关系或代理关系或任何法律或信托关系,或该公司是意法半导体的任何形式的关联公司。意法半导体合作伙伴计划的合作伙伴提供单独的许可,用于购买或使用其产品和/或服务以及与意法半导体设备相关的技术。请直接与适当的合作伙伴联系以获得许可条款、价格、支持和关于该合作伙伴的产品和/或服务的任何其他信息。这些产品和/或服务的条款和条件可能因合作伙伴而异,并可直接由该合作伙伴单独许可。意法半导体不对合作伙伴提供的产品和服务的适用性做出任何声明或保证,因此意法半导体特此明确拒绝合作伙伴提供的任何产品或服务的所有保证和条件,无论是明示的、默示的还是法定的,包括但不限于适销性、适用于特定目的、所有权、不侵权或因交易过程、使用或行业实践所产生的任何保证和条件。在任何情况下,意法半导体都不承担任何类型的直接、间接、附带、特殊、典型、后果性或惩罚性损害赔偿或其他损害赔偿,无论何种原因造成,包括但不限于使用损失、利润损失或收入损失,无论是基于合同责任理论、严格责任或侵权行为(包括疏忽或其他过失)提出的还是以何种方式产生的,或是与您参与或依赖合作伙伴计划,您使用或无法使用或购买合作伙伴的产品和/或服务,或产品和/或服务的性能,您与合作伙伴的关系,您使用或无法使用或依赖意法半导体门户网站或意法半导体在该门户网站上提供的任何信息有关的,即使意法半导体已被告知这些损害的可能性。与第三方网站的链接,如果由意法半导体提供,不受意法半导体的控制,意法半导体对链接网站的任何内容、材料、意见、建议或陈述或任何此类内容和材料的准确性或可靠性,以及链接网站中包含的任何链接,或对这些站点的任何更改或更新概不负责。意法半导体对从任何链接网站接收到的任何形式的传输概不负责,包括但不限于网络广播或音频传输。访问任何链接网站或链接网站中包含的任何链接的风险由用户自己承担。意法半导体提供这些链接只是为了方便,包含任何链接并不意味着意法半导体对第三方网站的任何保证(默示、明示或其他)或任何认可。
Actility is a global supplier of IoT connectivity solutions. Combining best-in-class LoRaWAN network servers with device & network management and added value services. Actility helps operators and enterprises to deploy IoT solutions for addressing vertical industries such as smart cities, logistics or the Industry 4.0.
With more than 100 million dollars raised in funding, Actility is the leader in LoRaWAN network deployments with more than 40 global clients including Orange, Proximus, KPN or Swisscom.
(#LoRaStarterPacks) (#STSECURE) (#STSAFE-A)
240
Amazon Web Service (AWS) IoT is a managed cloud platform that lets connected devices easily and securely interact with cloud applications and other devices. AWS IoT can support billions of devices and trillions of messages, and can process and route those messages to AWS endpoints and to other devices reliably and securely. With AWS IoT, your applications can keep track of and communicate with all your devices, all the time, even when they aren’t connected.
240
Jorjin Technologies is a provider of modular processing, sensing and wireless connectivity solutions, which enable our customers to bring innovative products to market fast with competitive cost. Jorjin wireless system in package (SiP) modules targeting wearable consumer electronics, automotive infotainment, cloud connected devices, and industrial mobile computing market.
Jorjin cover wide range of protocols including Wi-Fi, Bluetooth, ZigBee, WiSun, NFC, GPS, and GLONASS. In addition to supplying hardware, Jorjin offers driver porting services onto a wide range of application processors; Jorjin as well provide MCU-based connectivity solutions to support the emerging Internet of things (IoT) market. Jorjin hold advanced technology: producing extremely small footprints modules using either package on package (PoP) or multi-chip module (MCM) assembly technique.
Jorjin recently also set up a new imaging team to design and supply a range of camera sensor modules, 3D time of flight cameras and other sensor solutions to build up smart glasses for various industries applications.
(#STSAFE-A) (#STSECURE)
240
Transform your business with Internet of Things.
Build things : IoT begins with your things. Build with your things, from adding sensors to creating smart devices, to start your IoT solution.
Control your things : Deploy IoT solutions that control, monitor, and manage your things, allowing you to capture real-time data.
Analyze data : Take the data you collect and apply advanced analytics to uncover new business insights.
Act on insights : Transform insights into action through powerful applications—creating new revenue and business opportunities.
(#STSAFE-A) (#STSAFE-J) (#STSAFE-TPM) (#STSECURE)
240
Mocana’s end-to-end cybersecurity system protects millions of industrial control systems and smart connected devices that comprise the Internet of Things across all sectors.
"Mocana" means to set free, and our mission is to protect countries, cities, and families by enabling devices of every kind to be trustworthy and run securely and freely. Mocana was founded in 2002 to help protect military aircraft, vehicles, and devices. Our security software protects devices by using cryptography designed to run on microcontrollers and embedded devices. Today, we serve both the defense and commercial sectors.
Mocana is now running on every type of device you can imagine: fighter jets, helicopters, tanks, commercial aircraft, industrial automation and controls, thermostats, surveillance cameras, network gateways, set top boxes, medical devices, and much more. In fact, we now protect more than 100 million devices.
200 of the largest industrial manufacturing, aerospace, defense, utilities, energy, and transportation companies trust Mocana to harden their mission-critical devices and secure IoT communications using Mocana TrustPoint, our embedded IoT endpoint software, and Mocana TrustCenter, our automated security services platform. Our solutions enable our customers to secure their manufacturing supply chain.
Together, let's secure the Internet of Things from the inside out.
(#STSAFE-A) (#STSAFE-J) (#STSAFE-TPM) (#STSECURE)
240
总部位于上海的庆科信息技术有限公司是一家无线系统解决方案公司,为物联网应用提供独一无二的无线产品。成立于2004年的庆科信息已经掌握了成熟的无线技术,致力于为无线应用打造低功耗、安全、高性能的产品。
庆科信息从2007年开始专注于嵌入式系统开发。随后,该公司基于STM32 MCU推出了型号多样的无线模块,广泛覆盖智能家居、智能楼宇、智能照明、工业等特定垂直市场。庆科信息在业内率先推出基于微控制器的互联网连接操作系统MiCO,帮助开发者灵活设计充满创意的智能产品。2013年,庆科信息推出集成了STM32F411的EMW3165模块,深受市场欢迎,出货量突破100万。2017年,它推出最新的EMB1061,使用ST BlueNRG-1实现了对公用事业和工业系统的无线监测和控制。
庆科信息提供完整的端到端无线解决方案,包括无线模块、物联网操作系统MiCO、移动应用开发和云服务平台(便于第三方访问公共云或协议访问)等广泛的产品组合。庆科信息的单站方法使其能够提供最佳无线解决方案,在一个理想的基准点满足客户需求。我们的使命是使尚未互联的事物实现互联,让我们的生活更智能、更简单、更精彩。
(#STSAFE-A) (#STSECURE))
240
Sigfox, it’s about connecting the unconnected!
An inexpensive, long distance and lower power solution that's primed for multiple industrial & consumer applications.
Through its global LPWA network and rich ecosystem of expert partners, Sigfox delivers out-of-the box, two-way, secured communication services to unlock the true potential of the Internet of Things (IoT).
Sigfox provides a standard way of collecting data from sensors and devices with a single, standard-based set of APIs.
Besides, the Sigfox disruptive technology complements traditional cellular M2M by enabling global, ubiquitous, ultra-long battery life solutions at the lowest cost.
(#STSAFE-A) (#STSECURE)
240
The wolfSSL embedded SSL library is a lightweight, portable, C-language-based SSL/TLS library targeted at IoT, embedded, and RTOS environments primarily because of its size, speed, and feature set. It works seamlessly in desktop, enterprise, and cloud environments as well. wolfSSL supports industry standards up to the current TLS 1.3 and DTLS 1.2, is up to 20 times smaller than OpenSSL, offers a simple API, an OpenSSL compatibility layer, OCSP and CRL support, is backed by the robust wolfCrypt cryptography library, and much more.
The CMVP has issued FIPS 140-2 Certificates #3389 and #2425 for the wolfCrypt Module developed by wolfSSL Inc. For more information, see our FIPS FAQ.
Webinar
Webinar to learn how wolfSSL software can easily be integrated in STM32Cube projects
(#STSAFE-A) (#STSAFE-J) (#STSAFE-TPM) (#STSECURE)
240
如何提交您加入意法半导体合作伙伴计划的请求
意法半导体合作伙伴计划向在利用意法半导体组件设计产品、解决方案和服务方面具有成熟专业知识的公司开放。
这些公司必须与意法半导体人员(“意法半导体合作伙伴赞助商”)建立良好的关系,它们将成为您提交加入该计划的请求的主要接口。
必须提供以下信息才能让意法半导体团队根据合作伙伴成员资格认证流程来评估您的申请:
- 您的主要意法半导体联系人,“意法半导体合作伙伴赞助商”,与您密切合作的意法半导体员工,如业务开发、销售或营销人员
- 公司简介和提供的关键产品/服务的简短描述。这些信息将用于ST.com网站上的公司页面等多种通信材料,因此请注意提供有意义且正确的描述
- 与意法半导体器件有关的公司产品和服务的简短详细描述
- 业务信息,包括经营年限、年收入(如有可能)、员工人数和法律实体
- 公司总部的完整地址、两位主要联系人、公司网址和公司徽标(高分辨率)
- 公司运营国
一旦您参与该计划的申请获得批准,即会在两家公司都签署了落实合作领域的“营销协议”后,授予成员资格。
成员资格有效期为两年。有效期结束时,将会通过审查过程进行关系评估。
有关任何其他信息,您可以通过以下方式联系我们: partner.program@st.com