Fieldscale provides state-of-the-art simulation software for companies involved in the touch sensor industry all around the globe.
With Fieldscale, companies can:
- Reduce product development cycle and decrease time to market.
- Validate the performance of the design against customer requirements and reach the optimal design substantially faster.
- Test virtually a variety of different components from SENSE’s library under different environmental conditions without manufacturing costly hardware prototypes.
- Access cloud resources and analyze touch sensor designs on system-level in unprecedented speed.
Fieldscale expands the boundaries of electric simulation as we know them today, enabling very complex simulations since 2015.
Software offered by Fieldscale
Fieldscale is the company behind SENSE.
SENSE is a state-of-the-art capacitive touch sensor cloud simulation software, for electrical design and analysis, built from ground-up to support the constantly growing demands of engineers for accuracy and efficiency.
It features the unique capability to build an overall system configuration that closely replicates real-world performances by analyzing the touch sensor together with the MCU as a system.
Fieldscale in STMicroelectronics Ecosystem
STMicroelectronics worked together with Fieldscale to bring the electrical models of the Touch Sensing Controller peripheral of STM32 MCUs in SENSE. Users need simply to select their STM32 MCU and the software generates models for pin configurations, clock settings, and other parameters, such as charge and discharge cycles, among others. You can read our use case to see how an STM32 user can work with SENSE.
Traditionally, creating a capacitive touch sensing application is quite complicated and requires significant expertise. STMicroelectronics and Fieldscale simplify this process since engineers no longer need to produce multiple PCBs to see how a design works. They can validate the performance of an STM32 microcontroller and then they can implement their parameters into STM32CubeMX to write their application.
SENSE is essential for the STM32 microcontrollers' ecosystem.
Fieldscale enables STM32 users to select the Touch Sensor Controller module embedded in an STM32 MCU. They can configure its parameters and get virtually the equivalent circuit of any touch sensor in a netlist format. Then they can combine them together in a system level analysis to simulate the Raw Counts from the STM32 microcontroller just as they would be measured in the lab.
Before committing to building physical prototypes, with Fieldscale SENSE STM32 customers can validate the performance of their touch sensor designs by following simple steps:
- Design or import capacitive touch sensor layout as a standard DXF or Gerber file(s).
- Evaluate the Touch Sensor by extracting results about the Sensitivity, Capacitance and Resistance.
- Analyze the effect of any pointer touching at any location of the design, including finger, bare or gloved, and stylus.
- Identify and correct EMI related problems. Add RF conducted noise into the system, to simulate the testing procedure as specified in the IEC61000-4-6 standard, to evaluate the noise immunity of your system.
Fieldscale: Related Resources

产品和服务范围:
• 软件开发工具
公司总部地址:
45 N.Plastira str, 54250, Thessaloniki, Greece
公司主要联系人:
info@fieldscale.com
公司网站:
www.fieldscale.com
合作伙伴产品 | 描述 | 相关意法半导体产品 |
---|---|---|
SENSE | End-to-end solution for the design & system-level simulation of capacitive touch sensors | STM8L Series STM32L1 Series STM32WB Series STM32F3 Series STM32F0 Series STM32L0 Series STM32L4+ Series STM32L5 Series STM32L4 Series |
法律免责声明
除了本网站所载的使用条款、意法半导体销售条款和条件以及隐私政策,以下条款和条件适用于所有意法半导体合作伙伴计划。
尽管意法半导体已经尝试在网站上提供准确的信息,但意法半导体对信息的准确性不承担任何责任。意法半导体在本网站提供的所有信息均按“原样”提供,并包括所有错误,且无任何形式的保证,无论是明示的、默示的还是法定的。意法半导体可能随时更改或停止其合作伙伴计划或其产品或服务,恕不另行通知。对于非意法半导体产品或服务的任何提述仅供参考,不构成意法半导体的认可。在本网站上使用“合作伙伴”一词不表示或暗示意法半导体与任何其他公司之间存在任何合作伙伴关系或代理关系或任何法律或信托关系,或该公司是意法半导体的任何形式的关联公司。意法半导体合作伙伴计划的合作伙伴提供单独的许可,用于购买或使用其产品和/或服务以及与意法半导体设备相关的技术。请直接与适当的合作伙伴联系以获得许可条款、价格、支持和关于该合作伙伴的产品和/或服务的任何其他信息。这些产品和/或服务的条款和条件可能因合作伙伴而异,并可直接由该合作伙伴单独许可。意法半导体不对合作伙伴提供的产品和服务的适用性做出任何声明或保证,因此意法半导体特此明确拒绝合作伙伴提供的任何产品或服务的所有保证和条件,无论是明示的、默示的还是法定的,包括但不限于适销性、适用于特定目的、所有权、不侵权或因交易过程、使用或行业实践所产生的任何保证和条件。在任何情况下,意法半导体都不承担任何类型的直接、间接、附带、特殊、典型、后果性或惩罚性损害赔偿或其他损害赔偿,无论何种原因造成,包括但不限于使用损失、利润损失或收入损失,无论是基于合同责任理论、严格责任或侵权行为(包括疏忽或其他过失)提出的还是以何种方式产生的,或是与您参与或依赖合作伙伴计划,您使用或无法使用或购买合作伙伴的产品和/或服务,或产品和/或服务的性能,您与合作伙伴的关系,您使用或无法使用或依赖意法半导体门户网站或意法半导体在该门户网站上提供的任何信息有关的,即使意法半导体已被告知这些损害的可能性。与第三方网站的链接,如果由意法半导体提供,不受意法半导体的控制,意法半导体对链接网站的任何内容、材料、意见、建议或陈述或任何此类内容和材料的准确性或可靠性,以及链接网站中包含的任何链接,或对这些站点的任何更改或更新概不负责。意法半导体对从任何链接网站接收到的任何形式的传输概不负责,包括但不限于网络广播或音频传输。访问任何链接网站或链接网站中包含的任何链接的风险由用户自己承担。意法半导体提供这些链接只是为了方便,包含任何链接并不意味着意法半导体对第三方网站的任何保证(默示、明示或其他)或任何认可。

You’re now leaving st.com and will be re-directed to our Partner’s website.
For the latest innovations and solutions from ST, sign up for our newsletters.