About HCC
HCC Embedded develops deeply embedded software components “out of context”, which ensures that they can be used as core elements of any system, including those engineered to meet stringent requirements for safety, quality and portability. Built on a foundation of quality, HCC has a product portfolio of more than 250 embedded components, with deep competencies in reliable flash management, fail-safe file systems, and IPv4/v6 networking stacks and their associated security protocols, as well as a comprehensive suite of USB host and function software. Since 2002, HCC has supplied these embedded software components to more than 2,000 companies globally in a wide range of industries including industrial, medical and automotive.
HCC has built its organization on quality (ISO 9001:2015 and ISO 27001 certified) to deliver quality solutions.
With the introduction of its SEooC, (Safety Elements out of Context), HCC is using its focus on developing reusable safety components to raise the standard of available embedded software elements even higher. The embedded world is changing rapidly in terms of the complexity of development environments and the complexity of the required solutions. HCC continues to evolve with this change and provides embedded solutions to help companies, across all industries and locations, meet these challenges.
Advanced Embedded Framework
HCC has developed more than 250 reusable software components for use in deeply embedded systems. To do this in a scalable way with consistent quality across these components, HCC has created its Advanced Embedded Framework (AEF), the standard to which all components are engineered. The AEF ensures that each component is independent from any particular architecture, RTOS or toolchain. It also prescribes levels of quality to the code and its interfaces, to ensure that there is a consistent “look and feel” across the product range.
HCC Embedded products are used, without modification, in thousands of customer projects with over 30 different RTOSes, in 8, 16, 32 and 64-bit systems, big- or little-endian, with many architectures and tool chains.
Integrated Projects
Over the past 17 years, HCC has built more than 2,000 projects where HCC engineers have integrated HCC embedded components with its customers’ designs. The advantage of this approach is that HCC experts perform the software implementation on the customer-agreed target system. In this way HCC provides its customers with a common platform for development and support. Customers are buying more than just software; they are engaging in a long-term engineering partnership.

产品和服务范围:
• 嵌入式软件
公司总部地址:
Vaci ut 76, Budapest H-1133,
Hungary
公司主要联系人:
sales@hcc-embedded.com
公司网站:
www.hcc-embedded.com
合作伙伴产品 | 描述 | 相关意法半导体产品 |
---|---|---|
HCC SMFS | HCC has taken the radical approach of defining a system built around the needs of smart-meters. Metering applications usually have well-defined record structures and HCC has used its extensive flash experience to take advantage of this. |
STM32 32-bit Arm Cortex MCUs
|
HCC IPSec/IKE | IPSec/IKE provides a robust approach to security in embedded applications such as cars, "point-of-sale" terminals, medical devices, industrial equipment and many others. |
STM32 32-bit Arm Cortex MCUs
|
HCC Fail-safe File System | STM32的所有Flash文件系统,具有容错机制,来自HCC Embedded |
STM8 8-bit MCUs
STM32 32-bit Arm Cortex MCUs |
HCC Embedded Encryption Manager (EEM) | Embedded Encryption Manager (EEM ) allows developers to secure embedded systems using multiple encryption or hash algorithms through a uniform interface. |
STM32 32-bit Arm Cortex MCUs
|
HCC MISRA TCP/IPv4 and IPv6 | STM32的TCP/IP v4或v6堆栈,来自HCC Embedded |
STM32 32-bit Arm Cortex MCUs
|
HCC TLS | Verifiable TLS: a highly optimized software module designed to provide secure network communications for embedded devices. |
STM32 32-bit Arm Cortex MCUs
|
HCC USB Stack | STM32的USB主机和设备堆栈,来自HCC Embedded |
STM32 32-bit Arm Cortex MCUs
|
HCC MQTT | MQTT is a small and efficient machine-to-machine protocol. |
STM32 32-bit Arm Cortex MCUs
|
HCC Bootloaders | STM32的存储、USB或串行自举加载程序,来自HCC Embedded |
STM8 8-bit MCUs
STM32 32-bit Arm Cortex MCUs |
HCC FAT File System | HCC is renowned for its deep knowledge of flash storage media. In embedded systems, it is not possible to achieve the required efficiency, performance or reliability with a single file system. |
STM8 8-bit MCUs
STM32 32-bit Arm Cortex MCUs |
HCC Nichestack | InterNiche Technologies has been a leader in embedded networking for more than 25 years. Now a part of HCC Embedded, Nichestack technology is a valuable resource for any embedded developer. |
STM32 32-bit Arm Cortex MCUs
|
法律免责声明
除了本网站所载的使用条款、意法半导体销售条款和条件以及隐私政策,以下条款和条件适用于所有意法半导体合作伙伴计划。
尽管意法半导体已经尝试在网站上提供准确的信息,但意法半导体对信息的准确性不承担任何责任。意法半导体在本网站提供的所有信息均按“原样”提供,并包括所有错误,且无任何形式的保证,无论是明示的、默示的还是法定的。意法半导体可能随时更改或停止其合作伙伴计划或其产品或服务,恕不另行通知。对于非意法半导体产品或服务的任何提述仅供参考,不构成意法半导体的认可。在本网站上使用“合作伙伴”一词不表示或暗示意法半导体与任何其他公司之间存在任何合作伙伴关系或代理关系或任何法律或信托关系,或该公司是意法半导体的任何形式的关联公司。意法半导体合作伙伴计划的合作伙伴提供单独的许可,用于购买或使用其产品和/或服务以及与意法半导体设备相关的技术。请直接与适当的合作伙伴联系以获得许可条款、价格、支持和关于该合作伙伴的产品和/或服务的任何其他信息。这些产品和/或服务的条款和条件可能因合作伙伴而异,并可直接由该合作伙伴单独许可。意法半导体不对合作伙伴提供的产品和服务的适用性做出任何声明或保证,因此意法半导体特此明确拒绝合作伙伴提供的任何产品或服务的所有保证和条件,无论是明示的、默示的还是法定的,包括但不限于适销性、适用于特定目的、所有权、不侵权或因交易过程、使用或行业实践所产生的任何保证和条件。在任何情况下,意法半导体都不承担任何类型的直接、间接、附带、特殊、典型、后果性或惩罚性损害赔偿或其他损害赔偿,无论何种原因造成,包括但不限于使用损失、利润损失或收入损失,无论是基于合同责任理论、严格责任或侵权行为(包括疏忽或其他过失)提出的还是以何种方式产生的,或是与您参与或依赖合作伙伴计划,您使用或无法使用或购买合作伙伴的产品和/或服务,或产品和/或服务的性能,您与合作伙伴的关系,您使用或无法使用或依赖意法半导体门户网站或意法半导体在该门户网站上提供的任何信息有关的,即使意法半导体已被告知这些损害的可能性。与第三方网站的链接,如果由意法半导体提供,不受意法半导体的控制,意法半导体对链接网站的任何内容、材料、意见、建议或陈述或任何此类内容和材料的准确性或可靠性,以及链接网站中包含的任何链接,或对这些站点的任何更改或更新概不负责。意法半导体对从任何链接网站接收到的任何形式的传输概不负责,包括但不限于网络广播或音频传输。访问任何链接网站或链接网站中包含的任何链接的风险由用户自己承担。意法半导体提供这些链接只是为了方便,包含任何链接并不意味着意法半导体对第三方网站的任何保证(默示、明示或其他)或任何认可。

You’re now leaving st.com and will be re-directed to our Partner’s website.
For the latest innovations and solutions from ST, sign up for our newsletters.