The WITTENSTEIN Group was established in 1948 and has grown into a stable and mature global technology company. Originally part of the aerospace group, WHIS is the Group’s centre of excellence for high integrity and safety critical embedded systems design. WHIS is first and foremost a Safety Engineering Company, a key differentiation in the RTOS market, as WHIS have direct experience developing safety critical applications.
WHIS engineers have a profound knowledge of safety critical development, and high integrity development life cycles are well and truly institutionalised within company working practices. Today our primary focus is the development and supply of mission and safety critical RTOS.WITTENSTEIN high integrity systems (WHIS) is a safety systems company that produces and supplies real time operating systems (RTOS) and platform solutions to the Medical, Automotive, Aerospace, and Industrial sectors, increasing application development efficiency whilst reducing risk through third party certification. Our product include:
- SAFERTOS® – the safety critical real time operating system pre-certified to IEC 61508 SIL3 by TÜV SÜD;
- OPENRTOS® - commercial licensing and support for the popular FreeRTOS™;
- Enhanced Security Module – For the highest security-critical environments, WHIS offers the Enhanced Security Module (ESM) to reinforce and strengthen the existing security of our RTOS;
- Board Support Packages, Middleware, and Safety Plugins;
- Training, Consultancy and Support to realise the potential of your design.
Our Relationship with FreeRTOS
WHIS leverage RTOS technology from FreeRTOS.org, the market leading embedded real time operating system. Richard Barry created FreeRTOS while an employee at WHIS. WHIS engineers worked closely with Richard, providing a safety critical upgrade to FreeRTOS, SAFERTOS, as well as the flexible commercial licensing, training, and support that FreeRTOS users needed. SAFERTOS is based on the functional model of FreeRTOS, however it has been completely redesigned by our team of safety experts. Our engineers took the FreeRTOS functional model, subjected it to a full HAZOP, identified all areas of weakness within the functional model and API, and generated a set of safety requirements. The resulting functional and safety requirements sets were put through an IEC 61508-3 SIL 3 development life cycle, the highest possible for a software only component, creating the SAFERTOS code base and Design Assurance Pack.
As FreeRTOS and RTOS share the same functional model upgrading is easy. Many of our customers prototype using the FreeRTOS kernel, and convert to SAFERTOS at the start of their formal development phase.
Included in our free downloads is a manual detailing how to upgrade from the FreeRTOS kernel to SAFERTOS in easy steps.
(#FuSa)

产品和服务范围:
• 嵌入式软件
公司总部地址:
Brown’s Court, Long Ashton Business Park, Yanley Lane, Long Ashton, Bristol, United Kingdom
公司主要联系人:
Salomea Paprotny, Salomea.Paprotny@wittenstein.co.uk
合作伙伴产品 | 描述 | 相关意法半导体产品 |
---|---|---|
WITTENSTEIN Safety Plugins | Safety plugins source and Design Assurance Pack | STM32 32-bit Arm Cortex MCUs X-CUBE-STL |
WITTENSTEIN Enhanced Security Module | Enhanced Security Module | STM32 32-bit Arm Cortex MCUs |
WITTENSTEIN SAFERTOS CORE | SAFERTOS CORE,需考虑安全性但无需认证的嵌入式系统RTOS | STM32 32-bit Arm Cortex MCUs X-CUBE-STL |
WITTENSTEIN OPENRTOS | OPENRTOS,WITTENSTEIN高完整性系统中的高性能RTOS | STM32 32-bit Arm Cortex MCUs |
WITTENSTEIN SAFERTOS | SAFERTOS,WITTENSTEIN高完整性系统中的安全关键型RTOS | STM32 32-bit Arm Cortex MCUs X-CUBE-STL |
WITTENSTEIN CONNECT Middleware | CONNECT中间件:WITTENSTEIN高完整性系统中的TCP/IP、USB和File System组件 | STM32 32-bit Arm Cortex MCUs |
法律免责声明
除了本网站所载的使用条款、意法半导体销售条款和条件以及隐私政策,以下条款和条件适用于所有意法半导体合作伙伴计划。
尽管意法半导体已经尝试在网站上提供准确的信息,但意法半导体对信息的准确性不承担任何责任。意法半导体在本网站提供的所有信息均按“原样”提供,并包括所有错误,且无任何形式的保证,无论是明示的、默示的还是法定的。意法半导体可能随时更改或停止其合作伙伴计划或其产品或服务,恕不另行通知。对于非意法半导体产品或服务的任何提述仅供参考,不构成意法半导体的认可。在本网站上使用“合作伙伴”一词不表示或暗示意法半导体与任何其他公司之间存在任何合作伙伴关系或代理关系或任何法律或信托关系,或该公司是意法半导体的任何形式的关联公司。意法半导体合作伙伴计划的合作伙伴提供单独的许可,用于购买或使用其产品和/或服务以及与意法半导体设备相关的技术。请直接与适当的合作伙伴联系以获得许可条款、价格、支持和关于该合作伙伴的产品和/或服务的任何其他信息。这些产品和/或服务的条款和条件可能因合作伙伴而异,并可直接由该合作伙伴单独许可。意法半导体不对合作伙伴提供的产品和服务的适用性做出任何声明或保证,因此意法半导体特此明确拒绝合作伙伴提供的任何产品或服务的所有保证和条件,无论是明示的、默示的还是法定的,包括但不限于适销性、适用于特定目的、所有权、不侵权或因交易过程、使用或行业实践所产生的任何保证和条件。在任何情况下,意法半导体都不承担任何类型的直接、间接、附带、特殊、典型、后果性或惩罚性损害赔偿或其他损害赔偿,无论何种原因造成,包括但不限于使用损失、利润损失或收入损失,无论是基于合同责任理论、严格责任或侵权行为(包括疏忽或其他过失)提出的还是以何种方式产生的,或是与您参与或依赖合作伙伴计划,您使用或无法使用或购买合作伙伴的产品和/或服务,或产品和/或服务的性能,您与合作伙伴的关系,您使用或无法使用或依赖意法半导体门户网站或意法半导体在该门户网站上提供的任何信息有关的,即使意法半导体已被告知这些损害的可能性。与第三方网站的链接,如果由意法半导体提供,不受意法半导体的控制,意法半导体对链接网站的任何内容、材料、意见、建议或陈述或任何此类内容和材料的准确性或可靠性,以及链接网站中包含的任何链接,或对这些站点的任何更改或更新概不负责。意法半导体对从任何链接网站接收到的任何形式的传输概不负责,包括但不限于网络广播或音频传输。访问任何链接网站或链接网站中包含的任何链接的风险由用户自己承担。意法半导体提供这些链接只是为了方便,包含任何链接并不意味着意法半导体对第三方网站的任何保证(默示、明示或其他)或任何认可。

You’re now leaving st.com and will be re-directed to our Partner’s website.
For the latest innovations and solutions from ST, sign up for our newsletters.