The location computation is based on the data from the Sigfox infrastructure, coming from several replicas of the same messages sent by a device and received by different base stations.
The method used is not based on flight time or signal Doppler shift, but on the signal strength (RSSI - Received Signal Stren- gth Indicator) using a probability model (the location with the highest probability is selected).
The Sigfox Geolocation service will evolve in 2017 to increase its accuracy by using Machine Learning technology.
许可类型 | 授权费 |
软件类型 | 中间件 |
可交付成果 | 源文件 |
演示版本 | 有 |
支持的MCU | STM32, BlueNRG-2 |
地点 |