X-CUBE-IAP-USART

批量生产
Design Win

使用USART嵌入式软件进行STM32Cube应用内编程(AN4657)

获取软件 下载数据摘要
概述
样片和购买
解决方案
文件
工具与软件
质量与可靠性
Partner products
Sales Briefcase
开始

产品概述

描述

An important requirement for most Flash-memory-based systems is the ability to update firmware when installed in the end product. This ability is referred to as in-application programming (IAP). The X-CUBE-IAP-USART firmware package contains the source code of IAP examples based on the STM32Cube.
For more details refer to application note AN4657.
  • 所有功能

    • Flash erase
    • Flash programming
    • UART communication using Ymodem protocol
    • Flash write protection configuration
    • Separating application from loader

获取软件