With 30 years of experience from projects and product development in life science, Prevas is a skilled partner in the development of medical technology products.
The life science industry is quickly developing and is becoming more sensitive to competition. It needs innovative, cost-effective products that make use of new and proven technology. Prevas has an excellent track record in developing prize winning instruments and medical technology equipment tailored for our customers. Moreover, Prevas’ office in Sundbyberg is ISO13485 certified.
Prevas has more than 30 years of experience in balancing between using new and proven technology in efficiently creating innovative products. Moreover, Prevas understands the importance of having the right balance between investments in the development of assay, consumables and instrument/devices, and the usability of a single product or as a platform for products.
Prevas offers specialists or complete set of resources for development an idea into serial production product, which includes software, hardware, mechanics, quality assurance, project management resources. With our specialized teams, Prevas also offers turn-key development of medical devices and analytical instruments.
To be able to be on the technology edge, Prevas has a broad and elaborated specialist and partner network.
建议的服务 | 其它 |
地点 |