NFC(近场通信)是一种可靠的技术,经过高效集成可以极大改善用户体验。
如果您能够掌握正确的做法,就能轻松避免早期使用者遇到的糟糕使用体验。这样,NFC技术就可以为用户发挥其全部潜力,而不是让他/她们弃用。
使用NFC技术必须能为用户提供好处,而不是使他/她们不愿意使用。
NFC(近场通信)是一种可靠的技术,经过高效集成可以极大改善用户体验。
如果您能够掌握正确的做法,就能轻松避免早期使用者遇到的糟糕使用体验。这样,NFC技术就可以为用户发挥其全部潜力,而不是让他/她们弃用。
使用NFC技术必须能为用户提供好处,而不是使他/她们不愿意使用。
NFC技术基于13.56 MHz无线通信协议,支持在两个相隔不超过10厘米且支持NFC功能的设备之间进行无线通信。
非常便捷,此连接不依赖于Wi-F、4G、LTE或类似的技术,而且使用它不需要任何成本:不需要用户具备熟练技能;不需要电池;在不使用读卡器时不会发出射频波(它是一种无源技术);随着NFC技术在智能手机中的普及应用,每个人都可以享用NFC带来的好处。
NFC Forum(促进NFC和设备合规性的行业协会)帮助简化和标准化NFC的使用,以便为消费者提供便利。
NFC Forum称,在2020年初,地球上四分之一的居民(20亿人)拥有支持NFC功能的设备。每秒大约生产64台支持NFC功能的设备。这些设备通常是配备了NFC技术的智能手机。
下面这张图片显示许多行业在使用NFC技术及其应用。
Near Field Communication, or NFC, is a wireless technology that lets two devices connect when they are brought within a few centimeters of each other. NFC makes use of radio frequency identification (RFID) to transmit data. It follows protocols set by the NFC Forum, an industry group managing standards.
The great advantage of NFC is that it is very simple to use - just tap or wave devices together. No need for manual pairing. This makes it great for mobile payments, quickly sharing contacts or links and other tasks. While payments are the most common use today, NFC has many other applications too. It can be used to pair headphones, access public transit or share files.
NFC relies on a combination of two distinct technologies – Radio Frequency IDentification (RFID) and Near Field Communication (NFC). RFID refers to the technology that enables the reader or writer to detect the other device within its range. NFC refers to the protocols and standards developed by the NFC Forum that ensure the devices can actually communicate with each other. Together, these two technologies form the foundation of any successful NFC transaction.
NFC technology is being utilized in many different ways, including for payments, data transfer, access control, and authentication.
Sorry! Your browser is out-of-date
This browser is out of date and not supported by st.com.
As a result, you may be unable to access certain features.
Consider that modern browsers:
So why not taking the opportunity to update your browser and see this site correctly?