滤波器

ePOS和零售

STM32L5 MCU Series: Excellence in Ultra-Low-Power with More Security (6:41)

Security has emerged as one of the 3 key areas that developers of embedded and IoT applications are thriving to improve. The STM32L5 microcontroller series is the solution and provide a new optimal balance between performance, power and security. The STM32L5 MCU series harnesses the security features of the Arm Cortex-M33 processor and its TrustZone for Armv8-M combined with ST security implementation. ST-proprietary ultra-low-power technologies create a class-leading MCU for energy-conscious applications such as Internet of things (IoT), medical, industrial and consumer. Offering up to 512 Kbytes of flash (dual bank) memory and 256 Kbytes of SRAM, the STM32L5 series of microcontrollers reaches an upgraded level of performance (427 CoreMark) thanks to this new core and a new ST ART Accelerator™ (supporting now also external memory). The STM32L5 offers a large portfolio with 7 packages (from 48 to 144 pins) and supports up to 125°C ambient temperature.


×