The customer in order to use/instantiate this component has to perform the following tasks:

1)	Install the encrypted library on his ADS workspace:
from the main ADS window select "DesignKits" -> "Unzip Design Kit" therefore link the
RHFL4913A_ADS_EOR_MACROMODEL_ENCRYPTED_DESIGN_KIT.zip archive and specify the destination folder
where the archive has to be unzipped: after that select yes when ADS prompts if the customer wants to add
the unzipped library to the current customer workspace;

2)	After 1) the customer can select the component RHFL4913A_ADS_lib_EOR_MACROMODEL_schematic
from the added  library  RHFL4913A_ADS_EOR_MACROMODEL_ENCRYPTED_DESIGN_KIT and instantiate them
on his schematic.