The customer in order to use/instantiate this component has to perform the following tasks:

1) Install the encrypted library on his ADS workspace: 
from the main ADS window select DesignKits -> Unzip Design Kit therefore link the 
RHFL6000A_ADS_BOL_MACROMODEL_ENCRYPTED_DESIGN_KIT.zip archive and specify the destination folder 
where the archive has to be unzipped: after that select yes when ADS prompts if the customer wants to add 
the unzipped library to the current customer workspace;

2) After 1) the customer can select the component RHFL6000A_ADS_lib_BOL_MACROMODEL_schematic
from the added  library  RHFL6000A_ADS_BOL_MACROMODEL_ENCRYPTED_DESIGN_KIT and instantiate it 
on his schematic.