概述
产品选择器
解决方案
Documentation
CAD Resources
工具与软件
eDesignSuite
开始

意法半导体的运算放大器产品组合提供众多独特的高性能、低功率和精密运算放大器,采用微型封装。其电压范围为1.5 V至44 V,工作温度范围为-40至150°C。

为什么要选择意法半导体运算放大器

意法半导体运算放大器
  • 市面上最庞大的微功率运算放大器产品系列,功耗低至600 nA
  • 高可靠性、高产能的标准及高性能运算放大器供应商
  • 节省空间的封装,如CSP、DFN、QFN、SOT-23和SC-70

免费的在线研讨会
运算放大器:精确放大微弱信号

立刻免费访问我们录制的在线研讨会(50分钟),内容包括:

  • 运算放大器基础知识
  • 影响运算放大器精度的关键参数
  • 零漂移vs.标准精密放大器 - 优点和缺点
  • 意法半导体的运算放大器产品线和主打产品
  • 其他关键运算放大器参数

立刻前往在线研讨会

种类繁多的运算放大器

了解我们为应对工业、汽车和消费市场挑战而设计的种类越来越多的运算放大器。

10年长期供货计划
  • 低功耗运算放大器

    电流消耗极低的运算放大器,延长电池寿命,适合大量不同的应用。

  • 高精度运算放大器

    意法半导体的精密运算放大器解决方案包含零漂移放大器和温度范围内偏移漂移小的放大器。可与任何传感器完美配合使用,包括气体、温度、压力和位置传感器。

  • 低输入偏置电流运算放大器

    我们的系列产品适合任何跨阻抗应用或处理高阻抗传感器的应用。

  • 轨到轨运算放大器

    我们的轨到轨运算放大器产品包含几个系列,具有不同的电压范围及多种功耗和增益带宽组合。

  • 高电压运算放大器

    我们的高电压系列产品具有从2.7 V到36 V的扩展电源电压范围,简化了各种汽车和工业应用的设计:滤波器、电源和电机控制、执行器驱动、霍尔效应传感器和电阻式换能器。

  • 高速运算放大器

    意法半导体提供高端、高速运算放大器产品组合。

面向汽车应用

汽车运算放大器

了解我们的汽车级运算放大器产品组合,这些产品具有汽车应用所需的极高可靠性和质量。

查看所有汽车运算放大器

PDF - 快速参考指南

下载这个非常实用的PDF资源,包括:

  • 我如何为应用选择正确的运算放大器?
  • 典型运算放大器应用和关键参数
  • 使用意法半导体Op Amps应用程序一步步选择运算放大器
  • 意法半导体的运算放大器命名惯例
  • 词汇表
运算放大器pdf指南

意法半导体的运算放大器系列一览


operational amplifier portfolio

Questions / Answers around Op-Amps

What is op-amp offset voltage?

When a zero differential input voltage is applied, the op-amp output voltage should be zero. In practice, this is not the case. The offset voltage by definition is the differential input voltage that is required to make the output voltage zero.

What is op-amp input offset voltage?

The input offset voltage parameter, generally called VIO, is defined as a DC voltage between the non-inverting and the inverting input. It is always specified in the electrical characteristics of a datasheet. It can be positive or negative.

input offset voltage
Low input offset voltage VIO is key for high precision

The VIO value will be different for each op-amp. And to ensure good precision, it is important to choose the op-amp with the lowest VIO, because the VIO will be amplified by the gain and added to the total output voltage as an error.

Some op-amps with a chopper architecture like ST's TSZ121 exhibit a VIO of 5 µV. They are especially good for precision DC measurements.

What is input bias current of an operational amplifier?

Input bias current (IB) is the current flowing through an op-amp's inputs. Due to op-amp biasing requirements and normal operation leakage, a very small amount of current (pA or nA range, depending on the technology) is flowing through its inputs. This can cause issues when large value resistors or sources with higher output impedances are connected at the op-amp inputs. This leads to relevant voltage drops at the op-amp input and therefore errors.

What do rail-to-rail input and output mean for an op-amp?

An op-amp with a high rail input is able to deal with input signals up to +VCC. While a low rail input is able to deal with signals down to -VCC. Rail-to-rail input op-amps can handle input signals from -VCC to +VCC. Rail-to-rail output is the capability of an op-amp to drive its output very close to the power supply rails.