The Flasher ATE is a gang programmer suited for high volume mass production environments. The modular system uses a communication main board at its heart, that distributes the commands received from an ATE or a similar automated production handler system to the programming modules. Each programming module can be set up with individual configurations and firmware. The gang programmer is capable to program multiple devices in parallel, whether these devices are equal or part of a multi-device system, Flasher ATE can handle all production setups.
Key Features
Gang programmer
Scalable solution with up to 10 individual channels