STSW-WISE-STUDIO

批量生产
Design Win

WiSE-Studio free IDE for Windows, Linux, MAC OS

获取软件 下载数据摘要
概述
样片和购买
解决方案
文件
工具与软件
质量与可靠性
Partner products
Sales Briefcase
开始

产品概述

描述

The STSW-WISE-STUDIO package provides the WiSE-Studio Eclipse IDE, GCC toolchain based, supporting the BlueNRG-x Bluetooth Low Energy systems-on-chips (BlueNRG-1, BlueNRG-2 and BlueNRG-LP) and associated evaluation platforms.

The WiSE-STUDIO toolchain is provided free of charge for the user and it is based on standard GCC C/C++ compiler.

The tool offers an IDE environment allowing a specific user application to be built for the selected device, defining all the specific compile, assembler and linker options and to compile and run the application on the associated target device.

Furthermore, the tool offers standard debug capabilities to debug the user application through the selected SWD channel. CMSIS-DAP, J-Link, ST-Link/V2 are the supported SWD HW channels provided that the specific tool does not add any specific filter on the supported device.

For more information on how to use the tool, please refer to the “Quick start” section provided under “WiSE-Studio User Guide” in the Help menu of the tool.

  • 所有功能

    • Eclipse IDE for the BlueNRG-LP, BlueNRG-1, BlueNRG-2 SoC devices
    • Support for the BlueNRG-LP, BlueNRG-1, BlueNRG-2 evaluation platforms
    • GCC C/C++ compiler
    • GDB-based debugger
    • SWD channel support
    • No code size limit and free of charge
    • OS support: Windows

获取软件