Integrating ST’s comprehensive portfolio with NVIDIA’s Holoscan Sensor Bridge™ (HSB), NVIDIA Isaac Sim™ ecosystem and NVIDIA Halos for Robotics™
ST, in collaboration with NVIDIA, is empowering developers by simplifying and accelerating the creation of physical AI solutions. Through strengthened collaboration and tighter ecosystem integration, we are making it easier to design, train, and safely operate humanoid robots and other physical AI systems.
Integration with HSB, high-fidelity modeling and safety with NVIDIA Halos
As part of the collaboration, ST is working with NVIDIA to integrate its comprehensive portfolio with NVIDIA Holoscan Sensor Bridge. This includes HSB running on STM32 microcontrollers, inertial measurement units (IMUs), image sensors, time-of-flight (ToF devices), and motor-control solutions.
From a software perspective, high-fidelity NVIDIA Isaac models of ST components are being integrated into both companies’ robotics ecosystem.
Here are the first two tangible results of this engagement:
HW – HSB depth camera
The camera integrates a comprehensive set of ST sensors: two VB1940 RGBIR 5.1 MP image sensors for stereoscopic depth, a VL53L9CX ToF LiDAR module for standalone 3D depth mapping, and an LSM6DSV16X IMU for accurate positioning. Leopard's depth camera for robots is plug-and-play compatible with the Holoscan SDK via a 10G Ethernet interface. The camera can generate accurate 3D streams in low-power mode, with the option to engage host processing for higher-resolution depth maps and visualization. It is designed to support a broad range of robotic applications across physical AI platforms.
This enables developers to train vision, balance, gait, and motion control algorithms in simulation with confidence that these behaviors will transfer reliably to real hardware.
SW – ST high-fidelity MEMS sensor modeling
ST provides a high-fidelity model of its ASM330LHH IMU within NVIDIA Isaac Sim™, built from real device measurements including component-specific noise characteristics. The model provides a number of benefits for developers:
- Enables accurate virtual testing through direct integration with the simulator.
- Ensures balance and motion‑control algorithms behave consistently between simulation and real hardware.
- Uses the digital twin in Isaac Sim to let teams iterate on gait, balance, and navigation, reducing R&D effort.
Provides low‑latency sensor simulation to support the fast, stable responses required for complex humanoid movements.
- "ST is well engaged within the robotics community, providing robust support and a well-established ecosystem. Our collaboration with NVIDIA aims to unleash the next wave of cutting-edge robotics innovation with developer and customer experience streamlined at every step, from the inception of AI algorithms to the seamless integration of sensors and actuators. This will accelerate the evolution of sophisticated AI-driven physical platforms.”
- “Accelerating the development of next-generation autonomous systems requires high-fidelity simulation and seamless hardware integration to bridge the gap between virtual training and real-world deployment. The integration of STMicroelectronics’ sensor and actuator technologies with NVIDIA Isaac Sim, Holoscan Sensor Bridge and Jetson platforms provides developers with a unified foundation to build, simulate and deploy physical AI at scale.”
Extending the collaboration to NVIDIA Halos for Robotics
NVIDIA Halos for Robotics is a comprehensive safety system for industrial and humanoid robots. It comprises the NVIDIA IGX Thor™ and NVIDIA Holoscan Sensor Bridge, the NVIDIA Halos OS™, and the NVIDIA Halos AI Systems Inspection Lab. The NVIDIA Holoscan Sensor Bridge connects ST sensors and actuators to the NVIDIA computer platform. The NVIDIA Halos OS is the heart of the software stack and coordinates all the safety functions. And the NVIDIA Halos AI Systems Inspection Lab offers valuable assurance to industry leaders and regulators. As a Holoscan Sensor Bridge chip partner, ST is contributing to this end-to-end stack, joining the growing ecosystem that supports the platform and bringing the same sensing, processing, and actuation building blocks that streamline development in Isaac Sim and help robots operate safely around the people who work alongside them.
ST brings a long track record in functional safety to this effort. Several of its devices already meet automotive-grade requirements, including inertial measurement units compliant with ISO 26262 ASIL-B, and ST is now working to bring its HSB-ready STM32 microcontrollers, IMUs, image sensors, ToF sensors, motor control, and security solutions toward NVIDIA Halos readiness, across chips, evaluation kits, software, and reference designs. ST will also take part in the NVIDIA Halos AI Systems Inspection Lab, an accredited path that covers established and emerging safety standards, and looks forward to deepening its collaboration with NVIDIA as Halos for Robotics continues to evolve.
ST’s portfolio for robotics
ST offers one of the broadest semiconductor portfolios in the industry of components applicable to robotics - covering every major subsystem from edge AI processing and motor control to distributed sensing, power management, and secure connectivity. This integration depth means fewer vendors, faster system-level optimization, and a single partner across every major subsystem.
ST sensors for humanoid robotics
Humanoid robots depend on a wide range of sensing technologies to understand their surroundings, interpret movement, and interact naturally with people and objects. ST offers inertial, imaging, and depth sensing and is collaborating to create a developer-friendly ecosystem that supports robust perception and reliable sim-to-real performance.
Beyond providing accurate and rugged sensor hardware integrated with the Holoscan Sensor Bridge NVIDIA architecture, ST enhances the developer workflow through high-fidelity sensor models integrated into platforms like NVIDIA Isaac, helping ensure that behaviors trained in simulation translate seamlessly to physical robots.
ST’s portfolio and roadmap of AI enabled sensors further empowers edge intelligence, enabling faster reaction times and more fluid, lifelike motion across all parts of a humanoid robot.