![]() |
||
|
|
||
L'Oréal and STMicroelectronics applying semiconductors to skin aging |
||
Geneva, October 18, 2002 - STMicroelectronics and L'Oréal announced today the first use of semiconductors in the development of next-generation skin care. L'Oréal, a world leader in cosmetics, is using ST's TouchChip® silicon image sensor technology in an innovative research project to develop methods to quickly and easily provide detailed hydration analysis of human skin.The SkinChip® sensor, being jointly developed by the two companies, is based on ST's TouchChip®, developed for use in biometric fingerprint recognition applications. With over a quarter million units shipped, the TouchChip® is the most industrialized of the new generation of silicon sensors currently revolutionizing many security and convenience applications. The SkinChip® compact silicon sensor captures detailed, 500-dots/in. images of the skin in less than one-tenth of a second, under any skin or environmental conditions. The 90,000 active cells of the sensor provide high-quality image definition with a resolution of 50-microns, which is perfectly suitable for providing a detailed image of the micro-relief of skin. The sensor will be integrated into a compact device with low power consumption, suitable for portable application. ST's TouchChip®, on which the SkinChip® is based, is a capacitive sensor that uses active capacitive pixel sensing technology. When used in conjunction with specially developed image capture software, the sensor will generate a 'capacitance' map that can easily be converted into a hydration or dryness map. Assessing how dry or well-hydrated the skin is will allow L'Oréal to design beauty-care products better suited to age-related changes of skin. The two companies spent several months adapting the existing standard software used with the TouchChip®sensor in fingerprint applications to work on areas of human skin that are dryer than fingertips, such as on the face under the eyes, as well as jointly developing and optimizing image capture software to work with the sensor. Additionally, L'Oréal has further developed image analysis software for the application. The first software, developed by L'Oréal in conjunction with another research laboratory, detects orientations of lines in the micro-relief of the forearm. This parameter correlates to skin aging. Two further software programs are currently in development by L'Oréal: one for quantifying the actual hydration of the skin; and the second for measuring the 'texture' of the skin. According to L'Oréal, the SkinChip® sensor is currently being applied to cosmetics only, but could possibly be used in other dermatological applications in the future. "Because the TouchChip® provides a greyscale image of skin with unparalleled detail and sensitivity, it lends itself well to this unique and innovative application," said Alan Kramer, Director of ST's TouchChipÒ Business Unit. "L'Oréal's SkinChip® innovation promises to be a further advance in using leading-edge technology to help people look young." "The SkinChip® is an important new tool among non-invasive methods that will increase the knowledge of age-related skin changes and will allow us to greatly improve our ability to battle the effects of aging on appearance," according to Jean-Luc Lévêque, L'Oréal's Prospective Research Director. "L'Oréal's application of ST's sensor is a very exciting development." About L'Oréal Founded nearly a century ago by the chemist Eugène Schueller, L'Oréal has consistently applied its policy of investing in research, ensuring that its products meet the highest possible standards of quality, safety and innovation. Today, the L'Oréal Group contributes to the beauty of women and men all over the world, providing everyday solutions that enhance their sense of well-being.
About STMicroelectronics |
|
||||||||||||||||||
|