Section
 

STMicroelectronics' Kit to Power Enel's Next-Generation Electricity Meters


Geneva, November 3, 2004 - STMicroelectronics (NYSE: STM)
, one of the world's leading semiconductor manufacturers, has announced the release of a kit of semiconductor components for Enel's static electricity meters. Enel, one of the world's major electricity companies and the main operator in Italy, in 2001 launched a unique and challenging project in advanced automated meter management (AMM) system solutions and the fully supported ST kit has been produced to address this application.

"ST is proud to supply the complete kit of products and technologies that are required for this exciting application, from the critical power-line modem function to the microcontrollers, embedded memories, real-time clock chips, smart-power supply chips, and discrete devices that this application needs," said Enrico Villa, STMicroelectronics Corporate VP, Europe Region. "In addition, our specialised Competence Centers ensure that expert applications support is available world-wide to all customers working in the emerging field of remote metering."

The semiconductor component kit that ST is supplying reflects the company's strength as one of the world's leading broadline semiconductor manufacturers and its ability to reduce costs by offering complete kits fully supported by applications expertise. At the heart of the kit is ST's ST7538, the world's first single-chip power-line communications FSK (Frequency Shift Keying) transceiver, which integrates the FSK modem function that allows the meter to talk to the utility's offices, a power amplifier and a variety of frequency synthesis, core logic, voltage regulation, and input/output functions.

Another key component is the µPSD3200, a member of ST's family of Programmable System Devices that integrates a 40MHz, industry-standard microcontroller along with up to 288-kbytes of dual-bank Flash memory, 32-kbytes of SRAM, a Flash-based CPLD (Complex Programmable Logic Device) and a JTAG ISP (In-System Programming) interface to simplify testing. The µPSD3200 offers the world's largest memory densities for 8051-class microcontrollers.

The kit also includes the VIPer (Switched-Mode Power Supply) chip built with ST's proprietary VIPower smart-power technology and the M41T56M6, one of ST's many Low Power Consumption Real-Time Clock/Calendar devices that feature integrated battery switchover and write-protect functions plus software calibration for high-accuracy time-management features of the system.

Advertising Campaigns

About STMicroelectronics
STMicroelectronics is a global leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivalled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio and strategic partners positions the Company at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence markets. The Company's shares are traded on the New York Stock Exchange, on Euronext Paris and on the Milan Stock Exchange. In 2003, the Company's net revenues were $7.24 billion and net earnings were $253 million. Further information on ST can be found at www.st.com.


Should you require more information, please select the appropriate contact from the "Related Topics" menu.