![]() | ||
|
| ||
Smaller, Slimmer, and Smarter
- New Silicon Sensors from STMicroelectronics
| ||
Geneva,
October 12, 2005 – STMicroelectronics (NYSE: STM), a leading
supplier of MEMS (Micro-Electro-Mechanical System) devices, today announced
that it has expanded its portfolio of three-axis accelerometers with three
new models, embedding world-class performance in ever smaller packages.
From ultra-compact analog devices to ‘smart sensors’ with
two digital output formats (SPI/I2C), ST’s low-power, high-resolution
MEMS accelerometers address different system needs and hardware characteristics
in a wide range of low-g applications, from hard-disk drive protection
to motion user interfaces. ST’s LIS3LV02DQ is the market’s most advanced 3-axis low-g accelerometer with a standard SPI/I2C digital interface. Its novel features, including adjustable bandwidth and direction detection, mark the transition towards the concept of “smart sensors.” Adjustable bandwidth provides optimized performance for different frequencies, raising the resolution by eliminating interference from irrelevant frequency areas. In ST’s LIS3LV02DQ, the bandwidth can be flexibly changed with a software command, allowing designers to effectively combine measurements of slow and fast motions, such as tilts and vibrations, in one application. The embedded feature of direction detection immediately signals threshold crossing along any of the three axes. This information helps quickly understand in which direction the sensor is moving before any data calculations are made. Areas of application include intuitive user interfaces in various computer and consumer applications, such as 3D mice or gaming consoles. ST’s new analog-output LIS3L02AL/LIS3L06AL sensors are the market’s first devices in slim-and-small plastic LGA (Land Grid Array) packages. Their 5x5x1.5 mm3 dimensions meet the space constraints of the booming small-form-factor applications, including mini disc drives, mobile phones, and other portable electronic devices. ST’s leadership in MEMS miniaturization goes hand in hand with
superior performance parameters. The new accelerometers can measure
both tilt and acceleration along all three (x, y, z) axes at a very
low noise level and minimized power consumption, which is especially
critical in battery-operated portable systems. ST’s new three-axis analog sensor is available in two acceleration ranges, the standard +/- 2g LIS3L02AL for tilt applications, and a dynamically selectable choice of +/-2g and +/-6g in the LIS3L06AL, suited for measuring both static and dynamic accelerations, such as vibrations or rollover motions. “Shrinking dimensions, coupled with increasing performance, and embedded flexibility, open up a fascinating range of computer and consumer applications for our MEMS-based sensors,” said Hubert Geitner, Marketing and Business Development Manager at the MEMS Business Unit of ST. “ST’s silicon expertise and leadership in micro-machining technologies translate into the highest levels of sensitivity and robustness at very competitive prices. Furthermore, full ownership of the device manufacturing flow enables us to guarantee our customers long-term availability and roadmap continuity.” Available now in production volumes, unit pricing is $4.25 for the LIS3L02AL, $4.65 for the LIS3L06AL, and $5.35 for the LIS3LV02DQ, all for quantities of 10,000 pieces. About ST’s MEMS Portfolio About STMicroelectronics |
| |||||||||||||||||
|