Back in 1969, SGS, one of the two mother companies
of STMicroelectronics, introduced the first Power IC ever produced
in the World: the TAA611.
It was an Audio Power Amplifier capable of delivering 1W of power
over an 8 ohm load.
Since that time SGS, then SGS ATES, then SGS again, then SGS-THOMSON
and now STMicroelectronics has developed more than 100 different
Audio
Power Amplifiers.