NEWS
 

STMicroelectronics Expands Phone Camera Family with Highly Integrated 2-megapixel Module

Package options and on-chip features ensure wide acceptance of cost-effective, high-quality camera-phone imaging system

Click for larger image Geneva, February 05,2007 - STMicroelectronics (NYSE: STM), a world leader in CMOS imaging technology and the largest supplier of camera modules for mobile phones*, today announced a new 2-megapixel camera subsystem intended for the high-volume mainstream camera-phone market. The new VS6724 is the latest in ST’s camera-on-chip family, joining the successful 1.3-megapixel VS6624 and VGA-resolution VS6524 modules. It combines a high-quality multi-element lens with a 1/4-inch CMOS sensor and on-chip processing, in a tiny industry-standard package, to deliver superb UXGA-resolution (1600 x 1200 pixels) images.

ST addresses the varied demands of the competitive camera-phone market with a range of package and mechanical options. The VS6724 is available in super-low-profile 8 x 8 x 4.5mm and in high-performance 8 x 8 x 5.5mm SmOP2** packages, with both flex-cable attach and socket options for maximum design-in flexibility, the latter being compatible with industry-standard sockets. The camera has already been integrated successfully with major mobile phone platforms to minimize time-to-market for ST’s customers.

The camera delivers best-in-class, 30 frames per second UXGA-resolution output, for fast image capture, using an on-chip hardware M-JPEG (Motion - Joint Photographic Experts Group) encoder, or 15 fps YUV (Luminance-Bandwidth-Chrominance) output with no compression, through a fully-featured ISP (Image Signal Processing) pipeline. A flexible image scaling capability also provides an output for lower resolution displays; other features include image pan & tilt mode, and special effects such as sepia, negative and black & white. A highly configurable internal register set, with I2C interface, enables full customization of device behavior.

A video output stream to the ITU-R BT.656-4 standard, YUV (YCbCr) 4:2:2 with embedded sync, is provided, and an 8-bit parallel video interface with external horizontal and vertical synchronization signals. Output video formats are YUV 4:2:2, RGB (444 and 565), and M‑JPEG.

“The stunning images from this new camera module are the result of innovation both in high-quality, Imager-on-Chip CMOS technology, and in high-volume, optical package design and manufacture,” said Jean-Yves Gomez, General Manager of ST’s Imaging Division. “By controlling every phase in the design and manufacturing processes – something that’s unique in this market – ST can deliver excellent image quality in an easy-to-use product at a highly competitive price.”

In addition to its primary application in camera phones, the low-cost and industry-standard electrical interfaces and mechanical design make the VS6724 attractive for PDAs, gaming platforms, video conferencing and security cameras. Standby power consumption is ultra-low, and the device includes an on-board PLL (Phase Locked Loop) to support a wide range of input clock frequencies. The digital I/O can be powered from either 1.8V or 2.8V supplies.

The VS6724 is based on ST’s proprietary CMOS sensor technology and will be manufactured at the company’s leading-edge facilities in France, initially at Crolles and later on, also at Rousset. Samples of the VS6724 are available now, with volume production planned during the first quarter of 2007. Simple modules – not including socket or flex attach – are priced between $12.00 and $7.80 for volumes between 10,000 and 1 million pieces, respectively.

Click here for the high-resolution photo


About STMicroelectronics
STMicroelectronics is a global leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivalled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio and strategic partners positions the Company at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence markets. The Company's shares are traded on the New York Stock Exchange, on Euronext Paris and on the Milan Stock Exchange. In 2006, the Company's net revenues were $9.85 billion and net earnings were $782 million. Further information on ST can be found at www.st.com.
Information last updated Jan 2007




*      Based upon reports from TSR (Tokyo, September 2006) for shipments in the first half of 2006 and Prismark Partners LLC for shipments in 2005.

**   Small Optical Package, 2nd generation


Should you require more information, please select the appropriate contact from the "Related Topics" menu.