![]() | ||
|
| ||
STMicroelectronics’ New Nomadik® Chipset Boosts Multimedia Performance in Next-Generation Mobile Applications
| ||
Manufactured in ST’s 65nm low-power CMOS process, the STn8820 handles video at up to HD 720p resolution and plays all major standards, such as H.264 and VC-1, enabling video-on-the-go on any HDTV set. The embedded imaging engine produces high-quality still images at up to 8-megapixel resolution. The audio engines deliver days of music playback in hi-fi quality and the display and graphics engines enable 3D user interfaces and vivid gaming experiences by leveraging the OpenGL-ES2.0 geometry peak performance of 33 million Polygons per second.
With its high level of integration, the STw4820 reduces component costs and board-area requirements with no compromise in functionality. Compared with solutions based on several chips and discrete components, ST’s new audio and power manager saves as much as 30% of the Bill-of-Materials and 40% of the device footprint.
“ST’s Nomadik application processor brings consumer-device multimedia experience to wireless mobile devices,” said Monica de Virgiliis, General Manager of the Wireless Multimedia Division within ST’s Mobile, Multimedia & Communications Group. “The unique combination of superior processing performance with ultra-low power consumption will enable handset users to watch high-definition video in real time, play music in hi-fi quality, or immerse themselves in the life-like settings of a 3D world.” In addition to smart phones, ST’s new Nomadik chipset can be used in mobile Internet devices, mobile computers, portable multimedia and navigation devices, and in-car entertainment systems.
Samples of the new Nomadik chipset (STn8820 + STw4820) are available now, with volume production planned for Q4 2008. Chipset pricing is $37 each in quantities of 10,000. Click here for the STn8820 high-resolution photo Click here for the STw4820 high-resolution photo
|
| ||||||||||||||||||||
| |||||||||||||||||||||