NEWS
 

Silicon Carbide Schottky Diodes from STMicroelectronics Deliver Instant Efficiency Boost for Solar Power, Server Systems, Motor Controllers, and More

STPSC806D and STPSC1006D use latest substrate technology to eliminate power supply switching losses, improving efficiency and reducing heat

Click for larger image Geneva, February 09,2009 - Ordinary silicon diodes used in switched-mode power supplies lose up to 1% efficiency by not turning off immediately, but STMicroelectronics (NYSE: STM), a world leader in power semiconductors, is among the first companies to introduce silicon carbide (SiC) diodes that save this energy normally lost during switching.

The STPSC806D and STPSC1006D SiC Schottky diodes are especially useful in converters for solar power systems, where every fractional efficiency percentage is valuable. Power supplies for servers and telecom systems, which are operational round the clock, will also benefit from the cumulative savings of this apparently small improvement in efficiency. These diodes can also be used in motor controllers, which are deployed in large numbers worldwide, thereby saving the environmental impact of many thousands of Watts of generated energy.

Moreover, by saving the energy normally dissipated as heat by the silicon diode, the new SiC technology enables engineers to consider a lower maximum current rating for the diode. This allows smaller components to be used without sacrificing usable power. In high-power applications where heatsinks are normally used, these can also be made smaller leading to more compact power supplies delivering higher power density.

A further benefit for switched-mode power supply (SMPS) designers is that SiC diodes such as the STPSC806D and STPS1006D allow higher switching frequencies, which enable other components such as filtering capacitors and inductors to become smaller and less expensive, and consume less power.

SiC technology is able to deliver these benefits because no reverse recovery charge accumulates during the diode’s normal conduction period. When a conventional bipolar silicon diode is turned off, this charge must be dispelled by recombination between groups of charge carriers close to the diode junction. The current flowing during this recombination period is called the reverse recovery current. This undesired current, when combined with the voltage across associated semiconductor power switches, generates heat that will be dissipated by the switches. By eliminating this reverse recovery charge, SiC Schottky diodes have much lower switching losses across the board, leading to higher efficiency and lower heat dissipation.

The 8A-rated STPSC806D and 10A STPSC1006D, for 600V applications, are in full production in the industry-standard TO-220AC package, and available at $3.9 and $4.9, respectively, in quantities of 10,000.

Click here for the high-resolution photo


About STMicroelectronics
STMicroelectronics is a global leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivalled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio and strategic partners positions the Company at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence markets. The Company's shares are traded on the New York Stock Exchange, on Euronext Paris and on the Milan Stock Exchange. In 2008, the Company's net revenues were $9.84 billion. Further information on ST can be found at www.st.com.
Information last updated Jan 2009





Should you require more information, please select the appropriate contact from the "Related Topics" menu.