![]() | ||
|
| ||
STMicroelectronics Announces Smart Web Based Sensor Hardware Developer Kit from Arira Design for Active RFID Asset Monitoring and Security Applications
| ||
The Smart Web-Based Sensor HDK solves key technical challenges for companies seeking to develop wireless sensor networks for security and asset-monitoring applications. Developers can now blend standards-compliant active RFID with other wireless-networking and GPS capabilities and enhanced sensing features, exploiting built-in MEMS motion sensors and temperature and light sensors. The Smart Web Based Sensor HDK also enables longer battery life and smaller device sizes. “We strongly believe that the next big wave in sensors will be driven by the combination of the sensing function with wireless transmission – and ISO 18000-7 is the right solution for security and asset-monitoring applications,” said Benedetto Vigna, Group Vice President and General Manager of the MEMS and Healthcare Product Division at STMicroelectronics. “The Smart Web Based Sensor HDK is a best-in-class development platform that will help the adoption of wireless sensors across the industry. The HDK’s rich ecosystem of sensors, combined with Savi’s active RFID technology, will enable users to meet demanding technical and functional requirements.” “By making this Smart Web Based Sensor HDK available, STMicroelectronics has cleared a large hurdle for companies seeking to innovate with active RFID,” said David Shannon, senior vice president of Savi Technology, the world’s leading provider of active RFID products based on ISO 18000-7 standards. “The HDK enables innovators to quickly and inexpensively develop new products based on the global standard for active RFID and will help expand the market for active RFID.”
About the Smart Web Based Sensor HDK
Developed by engineers from ST’s Multi-Market Competence Center in Schaumburg, Illinois, in conjunction with Arira Design, based in Sunnyvale, California, the STM32 microcontroller-based platform is now being released in beta and is available from Arira Design via the web at http://www.ariradesign.com/hdk.php or by calling +1 408-789-2400.
About the ISO 18000-7 Standard
While Savi supports STMicroelectronics’ efforts to build this HDK, developers seeking to market or sell ISO 18000-7 compliant products are required to have a license from Savi, which owns the air interface protocol patent incorporated into the standard. For more information on Savi’s ISO 18000-7 licensing program, visit http://www.savi.com/licensingprogram-form.shtml or call +1 650-316-4936.
About Arira Design
|
| |||||||||||||||||||
| ||||||||||||||||||||