NEWS
 

STMicroelectronics Drives for Higher Performance with New 32-Mbit Flash Memory for Automotive Applications

New technology brings key features to M58BW32F, including low-voltage operation, higher performance, and a flexible protection scheme

Click for larger image Geneva, August 30,2006 - STMicroelectronics (NYSE: STM) today announced a new and enhanced version of its 32-Mbit Flash memory chip that is intended specifically for the automotive market. Offering high-speed memory access over a wide operating temperature range, the M58BW32F fits perfectly with automotive customers’ needs for powertrain and transmission-control modules, and for other high-performance automotive systems that use the latest generation of 32-bit microcontrollers.

The new M58BW32F is manufactured with an advanced 0.11-micron technology and benefits from ST's long experience as a leader in standalone and embedded Flash memory products. Automotive-Grade certified, and qualified to the AEC-Q100 standard (revision F) as defined by the Automotive Electronics Council, the new device uses a state-of-the-art architecture to reduce access times to as low as 45nsec over the full automotive temperature range (-40 degrees C to +125 degrees C for the packaged device, -40 degrees C to +150 degrees C in bare die form). Maximum burst frequency is 75MHz across the full temperature range.

The M58BW32F features a wide 32-bit data bus and operates on a nominal 3.3V memory core supply. Enhanced protection techniques include flexible hardware/software protection, a secured command set for Modify operations, a Bank Erase command and a one-shot program from an internal buffer (loaded up to an 8 x Double word maximum). For security, each die embeds a unique device ID to allow the use of cryptographic algorithms to protect against illegal software modifications.

The new automotive Flash memory is offered in an LBGA80 package, which uses ST’s ECOPACK RoHS-compliant lead-free technology, as well as in Certified Bare Die form. All devices are manufactured in ST facilities qualified to ISO/TS 16949:2002, and use ST’s volume-proven state-of-the-art manufacturing and testing technologies to offer reliable solutions for automotive applications.

Engineering samples are available for evaluation now, with volume production planned for Q3 2006. A 16-Mbit device is planned for the second half of 2006. Pricing for the M58BW32F is US$5.5 per device.

Further information is available at www.st.com/flashnor-embedded

Click here for the high-resolution photo


About STMicroelectronics
STMicroelectronics is a global leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivalled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio and strategic partners positions the Company at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence markets. The Company's shares are traded on the New York Stock Exchange, on Euronext Paris and on the Milan Stock Exchange. In 2005, the Company's net revenues were $8.88 billion and net earnings were $266 million. Further information on ST can be found at www.st.com.
Information last updated Jan 2006





Should you require more information, please select the appropriate contact from the "Related Topics" menu.