ST Life.augmented

Press Release

STMicroelectronics Sweeps Away Design Barriers with New STM32 Value-Line Microcontrollers Delivering 32 bits at 32 cents

STM32F030 Value Line with ARM® Cortex™-M0 brings 32-bit design advantages to price-conscious projects
Geneva /
Priced as low as $0.32 for high-volume orders, the latest STM32F030 Value Line microcontrollers from STMicroelectronics (NYSE: STM), a global semiconductor leader serving customers across the spectrum of electronics applications, are ideal for lower-budget projects while offering access to a full portfolio of hardware- and software-compatible 32-bit microcontrollers ideally suited for performance improvements and product extensions.

The new STM32F030 Value Line is based on the ARM® Cortex™-M0 core running at 48MHz. Unlike similar competing devices, the Value Line enables 8-bit price parity without compromising performance or features, such as a lower core speed or reduced peripherals.

“This new product line makes the benefits of 32-bit development more accessible to entry-level applications than ever before,” said Michel Buffa, General Manager Microcontroller Division, STMicroelectronics. “Engineers can work efficiently at a high level of abstraction and simplify their software by leveraging the enhanced hardware features. Access to the ARM developer community and ecosystem provide further incentives to move from the 8-bit world to the STM32 Value Line.”

Central to ST’s new Value Line concept is a strong base specification that effectively streamlines component selection and product differentiation. The STM32F030 line of products begins at 16KByte Flash and 4KByte RAM in a 20 pin package, and comprises a total of five parts up to 64KByte Flash, 8KByte RAM and 32, 48 or 64 pin packages. All variants feature a 12-bit 1Msample/s ADC, 1.2V internal reference, communication peripherals, temperature sensor and timers capable of supporting ADC synchronization, dead-time management, and PWM (Pulse-Width Modulation) timing for motor control. In addition to 48MHz core frequency, these rich peripherals set the STM32F030 Value Line apart from other entry-level 32-bit families. An internal RTC and 5-channel Direct Memory Access (DMA), which are features not typically available in other microcontrollers at this price level, also help ease application development and improve performance.

Moreover, developers gain entry to ST’s full portfolio of ARM Cortex-M microcontrollers, which includes more than 360 variants leveraging extensive pin, software and peripherals compatibility between Cortex-M0, M3 and M4 families.

ST is now taking sample orders for the STM32F030 Value Line. Volume production is planned to begin in Q3 2013.

About STMicroelectronics
ST is a global leader in the semiconductor market serving customers across the spectrum of sense and power and automotive products and embedded processing solutions. From energy management and savings to trust and data security, from healthcare and wellness to smart consumer devices, in the home, car and office, at work and at play, ST is found everywhere microelectronics make a positive and innovative contribution to people's life. By getting more from technology to get more from life, ST stands for life.augmented.

In 2012, the Company’s net revenues were $8.49 billion. Further information on ST can be found at

Feedback Form
Customer Feedback