ST Life.augmented

Press Release

STMicroelectronics Builds Wearable Technology Portfolio to Cement Market Leadership

Wave of analog and mixed-signal devices completes full collection for wearable applications 
Geneva /

STMicroelectronics (NYSE: STM), a global semiconductor leader serving customers across the spectrum of electronics applications, has announced a raft of analog and mixed-signal devices targeting the rapidly growing market for wearable technology.  These devices include current sensors, audio amplifiers, op amps, analog switches, and battery gas gauges enabling ST to offer the industry’s most complete set of building blocks for creating innovative wearable applications. 

 

Wearable applications are making a growing impact in markets that range from new healthcare technologies including remote heart-rate monitoring to consumer applications such as smart fashion accessories.  These applications represent a range of current and future markets that market analysts Strategy Analytics projects to grow by more than 70% through 2017.

“In conjunction with our industry-leading range of motion and environmental sensorsand our successes* in a broad range of already-available wearable applications, our newultra-low power microcontrollers, and our award-winningBlueNRG Bluetooth® Smart wireless connectivity solution, the analog and mixed-signal devices complete a comprehensive platform that makes ST the clear one-stop supplier of choice for customers developing innovative wearable applications,” said Andrea Onetti, General Manager Analog and Audio Systems Division, STMicroelectronics.

Examples of devices suitable for wearable applications include ST’s single, dual, and quad op amps, such as the OA4NP33 quad  low-power op amp, that offer an ultra-low-power typical consumption of just 580nA per channel (at 1.8V power supply), making them ideally suited for functions such as sensor signal-conditioning in battery-operated wearable devices. Another product, the GG25L gas gauge, uses a patented OptimGauge™ algorithm to monitor battery voltage to an accuracy of 0.25%.

Examples from ST’s rich portfolio of motion sensors include the LIS2DH12 ultra-low-power digital 3-axis accelerometer and the award-winningLSM303C ultra-compact high-performance e-compass module. ST’s M24SR dynamic tags add NFC connectivity to wearable applications for convenient wireless pairing, automatic connection to websites, or warranty-card activation.

All of the devices are available in volume from March 2014.

Click here for the high-resolution photo

 

About STMicroelectronics
ST is a global leader in the semiconductor market serving customers across the spectrum of sense and power and automotive products and embedded processing solutions. From energy management and savings to trust and data security, from healthcare and wellness to smart consumer devices, in the home, car and office, at work and at play, ST is found everywhere microelectronics make a positive and innovative contribution to people's life. By getting more from technology to get more from life, ST stands for life.augmented.

In 2013, the Company’s net revenues were $8.08 billion. Further information on ST can be found at www.st.com.

* Select previously issued press releases highlighting ST’s wearables successes:

 

1Source: IHS Consumer and Mobile MEMS Market Tracker H1 2013
2 STMicroelectronics Launches New STM32 Ultra-Low-Power Microcontrollers for Consumer, Health, and Industrial Applications
3 STMicroelectronics Receives Two 2014 CES Innovations Awards

4 LSM303C earned the Device of the Year recognition from MEMS Industry Group