ST Life.augmented

Car-ELE Japan 2013

Booth Info
ST demonstrates the execution as a leader in the growth drivers of Smart Power, MEMS and Sensors, Application Processors and Digital Consumer, Microcontrollers, and Automotive. 
Venue: Tokyo Big Sight, Japan

CAR-ELE JAPAN is Asia's largest trade show for automotive electronics where all kinds of related technologies such as components, materials, software and manufacturing & testing equipment gather. The show provides you with the best opportunities to meet automobile manufacturers and components manufacturers from all over Japan and Asia. Exhibit at CAR-ELE JAPAN to expand your business in Japan & Asia!


STMicroelectronics participated to CAR-ELE 2013 to confirm and illustrate our position as leading automotive components and solutions provider

STMicroelectronics exhibited and focused on following products

32bits automotive microcontrollers for chassis and safety
MCU families are members of a set of 32-bits Flash MCU dedicated to the specific needs of chassis and safety applications, with special focus on functional safety and advanced threephase motor control.
The unique modularity and scalability of their architecture provides compatible devices covering the wide range of chassis and safety applications with optimum cost, safety and performance trade-offs.
Wide range air fuel sensor control interface L9780
L9780 is an IC designed to interface a variety of
wide range air fuel sensors.
The device manages the oxygen pump of the
wide range air fuel sensor by means of a voltage
controlled current source (VCCS). The reference
for the VCCS is generated by a PI controller with
external compensation network in order to adapt
the device to different sensors.
http://jan2013.tems-system.com/exhisearch/show_image.aspx?id=483e82c3-e63b-4619-ba1c-8a8b07392d1b&item=71& data-cke-saved-name=photo.jpg name=photo.jpg
Host processor for cost-effective in-dash infotainment and telematics
ST's Cartesio+ application processor offers compact, innovative, cost-effective solutions for in-car navigation, head units and telematics boxes. Cartesio+ delivers boosted processing capability combined with leading-edge positioning, multimedia, 2D-3D GFX and connectivity technologies.http://jan2013.tems-system.com/exhisearch/show_image.aspx?id=483e82c3-e63b-4619-ba1c-8a8b07392d1b&item=86& data-cke-saved-name=zu.jpg name=zu.jpg
Automotive-grade MEMS sensor solutions
Housed in ultra-small packages and featuring excellent stability over time and temperature, ST's accelerometers are the ideal choice for all the most demanding automotive applications.
ST's latest gyroscopes feature excellent accuracy as a result of their unique and patented
mechanical structure based on a single driving mass.
http://jan2013.tems-system.com/exhisearch/show_image.aspx?id=483e82c3-e63b-4619-ba1c-8a8b07392d1b&item=101& data-cke-saved-name=zu2.jpg name=zu2.jpg