![]() |
||
| |
||
| ST Home | Corporate Responsibility | CR Report 2006 | Environmental Performance | Concrete Local Actions | Reducing Energy Needs in Singapore | ||
Corporate Responsibility Report 2006Environmental Performance |
||
Reducing energy needs in Ang Mo Kio site in SingaporeOur AMK Site has implemented more than 100 energy conservation projects (1994 to 2006) | EN7 |
1) Upgrade chilled water pumps AMK5” 2) Use scrubber water to pre-cool cooling tower water in AMK5” 3) Replace air handling unit with double coil in AMK5” 4) Upgrade condenser water pumps in AMK5” 5) “Power Planner” device on condenser water pumps in AMK6” 6) Solar Hot water system in AMK6” ST Singapore uses electricity generated from natural gas which pollutes less than oil. It also generates lower emissions of greenhouse gases, SOx and NOx to the environment. (*) ROI: Return On Investment |
|