ST has remained a constant driving force
in the Smartcard arena by investing continually in technology,
in research and development, in industrialization and by
creating partnerships on which secure solutions and applications
can be built. |
|
| |
25 years of Secure ICs
Experience |
|
| |
| 2006 |
Launch of 0.13µm ST21 optimized platform |
| 2005 |
First 0.18µm CMOS 128 K 32b smartcard
MCU EAL5+ Certification |
| 2003 |
Volume shipment of first 0.18µm 128K
32b Microcontroller for high-end SIM |
| 2002 |
First 32K C-less Microcontroller with
PKI EAL4+ Certified |
| 2001 |
Shipment of ST's 1 billionth Microcontroller
based Smartcard Device |
| 2000 |
First Common Criteria Security
Evaluation (EAL4 High) - ST19SFxx |
| 2000 |
First Contactless IC with 424kbit/s
Communication Interface |
| 1999 |
Demonstrated the first 32-bit JavacardTM
Smartcard (SmartJTM) |
| 1997 |
First MCU based Contactless Smartcard
IC - ST16RF42 |
1996 |
Shipment of ST's 1 billionth Memory/Smartcard
Device |
| 1994 |
First Smartcard IC with embedded Crypto-Accelerator |
| 1984 |
Development of MCU-based Smartcard IC
for Banking |
| 1982 |
First Secure Memory IC produced |
| 1981 |
Team created to design "Chip Cards" |
|
| |
To read more:
“STMicroelectronics:
25 Years at the Leading Edge of the Smartcard Industry - A Brief
History of STMicroelectronics in Smartcard” - B985M -
November 2006 |
| |
| Innovation |
The technologies required to cost effectively protect assets on
a chip-based card are both advanced and diverse. At ST we are constantly
researching into new techniques and technologies to ensure that
the next generation of Smartcard ICs are even more secure than their
predecessors. |
| |
| Security |
ST recognized early the importance of independent security evaluations
to internationally recognized standards. Years of focusing totally
on security have enabled us to stay at the forefront of independent
security evaluations (such as ISO 15408) and provide solutions for
specific corporate and governmental requirements.(more...) |
| |
| Strategic Partnerships |
ST has skillfully blended a powerful network of world-class Smartcard
partnerships. These include strategic alliances with key customers
and organizations, technology development alliances with customers,
CAD and IP providers, and, partnerships with universities, research
institutes and multinational R&D organizations.
From our first groundbreaking IC for phone cards through to our
revolutionary 32-bit SmartJ platform, ST has been writing Smartcard
history for over two decades.(more...) |
|
|