Company
ST Home | Sensors | Motion Sensors (MEMS)

Motion Sensors (MEMS)

Sensors based on MEMS (Micro-electro mechanical systems) technology are conquering many market segments, ranging from mobile communication and computing to consumer electronics, healthcare and industrial.
The average annual growth of MEMS market is more than 20%, that’s why is expected to reach $10 billions by 2010*, when analysts predict that every portable HDD-based device and mobile phone will contain a MEMS-based accelerometer.
 
In this scenario, ST is playing a major role, with a broad portfolio of multi-axis accelerometers already in high-volume production and hundred millions components delivered to the market.


The most challenging and forward-thinking test today is represented by the capability to discover and foresee new applications to entertain, amaze, and to protect the end user. That’s why ST is continuously investing in research and development of new MEMS-based products as gyroscopes, pressure sensors, microphones, and module solutions and it is establishing strategic partnerships with leading companies.

In addition, ST’s capability to match mass market requests is guarantee by the first state-of-the-art 8” silicon manufacturing line, with full ownership of manufacturing and testing flow, to properly accommodate the fast time-to-market required by the consumer market and guarantee long term products availability, high volumes in scale production and roadmap continuity.

(* ST estimate based on data from market research analysts In-Stat, Nexus and Yole Development.)

 
Motion Sensors (MEMS) Families
 
Applications

MEMS-based sensors are ideal for a wide array of applications in consumer, communication, automotive and industrial markets.

The consumer market has been a key driver for MEMS technology success. For example, in a mobile phone, MP3/MP4 player or PDA, these sensors offer a new intuitive motion-based approach to navigation within and between pages. In game controllers, MEMS sensors allow the player to play just moving the controller/pad; the sensor determines the motion rather than the player providing game input by pushing buttons. Another typical application in the consumer market is HDD protection; in the case of free fall, a MEMS sensor informs the hard disk control to park the head, saving the data prior to the shock when reaching the ground.

Another interesting driver market for MEMS-based sensors is the industrial one where MEMS sensors can be used for vibration monitoring and control. For example, vibrations can degrade dishwasher and washing machine performance and reduce the lifetime itself. MEMS sensors can be used to measure the vibrations and, as a result, identify potential machine problems prior to equipment failure, so allowing preventive maintenance to be implemented.

 
New Products
LIS344ALH: 3-axis, high performance ± 2g/± 6g ultra-compact accelerometer
LIS244ALH: 2-axis, high performance ± 2g/± 6g ultra-compact accelerometer
LIS344AL: 3-axis, ± 3.5g ultra-compact linear accelerometer
LIS331DL: 3-axis, ± 2g/± 8g smart motion sensor with digital output
LIS331AL: 3-axis, ± 2g motion sensor with analog output
LIS244AL: 2-axis - ± 2g ultra-compact linear accelerometer
 
Product News
Press announcement, June 11, 2008
STMicroelectronics’ New 3D Orientation Sensor Begins New Generation of Highly Integrated Functional Sensors using Robust MEMS Technology
Press announcement, June 09, 2008
STMicroelectronics Boosts MEMS Portfolio with New ‘Gyroscope’ Angular Rate Sensors Offering Extended Supply Voltage Range
Press announcement, april 21, 2008
STMicroelectronics to Highlight Convergence of Sensors and Wireless Technologies at M2M Forum 2008
Press announcement, april 15, 2008
STMicroelectronics Reinforces its Leadership in MEMS with New High-Performance Motion Sensors
Press announcement, january 8, 2008
ST’s MEMS Sensor Enables In-Air Motion Control in New PC and Media Remotes from Gyration
Press announcement, december 21, 2007
LIS344AL STMicroelectronics Announces Extra Degree of Freedom in 4 x 4mm Analog-Output Accelerometer Family
Press announcement, october 02, 2007
Smaller and Smarter Motion Sensors from STMicroelectronics Spearhead MEMS Consumerization
Press announcement, july 06, 2007
New Two-Axis Analog Accelerometer from STMicroelectronics Saves Space and Power in Portable Applications
See all
 
Brochures and product guides

MEMS (Selection guide, PDF)
MEMS linear accelerometers (A world of applications, PDF)
MEMS sensors for car alarm, crash recorder and more (Brochure, PDF)
LIS302DL (Brochure, PDF)

 
Related information

Articles and Papers

For further information, especially concerning new products, please do not hesitate to Contact Us