About ST
Products
Applications
Support
Buy
News & Events
ST Worldwide
Contact Us
Login
Application Notes
|
Cross-Industry
|
General Purpose Products
|
Timekeeper
|
Timekeepers
TIMEKEEPER® rolling into the year 2000 (21st century, Y2K)
Application Note
Format:
(19 kb)
or
(4 kb)
Last Updated: 20/02/2008
Pages: 2
Related Datasheets
5.0 or 3.3 V TIMEKEEPER® supervisor
5.0 or 3.3V, 256 Kbit (32 Kbit x 8) TIMEKEEPER® SRAM
5.0V PC real-time clock
5.0V, 16 Kbit (2Kb X 8) TIMEKEEPER SRAM
5.0V, 64 KBIT (8 KB X 8) TIMEKEEPER® SRAM
5V, 256 Kbit (32 Kb x 8) TIMEKEEPER® SRAM
5V, 64 Kbit (8 Kb X 8) TIMEKEEPER SRAM
64 Kbit (8 Kbit X 8) TIMEKEEPER® SRAM
Serial real-time clock with 56 bytes NVRAM
Raw Ascii Text
- (
Hide
)
(Unformatted textual content of the document used by search engines)
AN923 APPLICATION NOTE
TIMEKEEPER Rolling into the Year 2000 (21st Century, Y2K)
The members of the TIMEKEEPER family, from STMicroelectronics, are listed in Table 1. Each contains, in a single-package footprint, non-volatile RAM (NVRAM) and a real time clock (RTC), offering dedicated time-keeping and alarm functions. Table 1. Family of TIMEKEEPER Devices
M41T56 M48T86 M48T559 M48T02, M48T12, M48T08, M48T18, M48T58, M48T59, M48T35, M48T37 M48T201 Low cost RTC that is compatible with Serial I2C bus applications RTC primarily utilized for its timekeeping functions with little additional memory RTC with 64 Kbit memory that supports Address, Data Multiplexed I/O pins RTCs with 16 Kbit to 256 Kbit of additional asynchronous SRAM non-volatile memory TIMEKEEPER SUPERVISOR
CEN TURY ROLLOVER The date and time information is distributed over several internal registers, with two BCD digits in each register. Fabricated in ST's SRAM technology, the individual registers can be accessed by the user like a conventional bank of SRAM (read accesses to read the time, write accesses to set a new time). The year is divided into two fields: the Century field, and the Years field (each is 8 bits wide, holding two BCD digits). TIMEKEEPER devices that were designed in 1997, and after, have a register for each of these fields; those that were designed before 1997, though, do not have the Century register. At the turn of the century, all TIMEKEEPERS will increment the Years register from 99 to 00 (from 1001,1001 to 0000,0000). Those that have a Century register, will, at the same moment, increment it from 19 to 20 (from 0001,1001 to 0010,0000). The Century register, where present, is positioned 14 address locations before the most significant byte address, using the device's 16-byte register map definition. For a 32K x 8 device, for example, the Century register is at address location 7FF1h. For TIMEKEEPER devices that do not have a Century register, but which utilize the 16-byte register map definition, it is recommended that the user sets up the same location (location 7FF1h for a 32K x 8 device, for example) for storing the Century information. This byte, of course, is not updated automatically by the clock, but has to be updated manually by the user's software. It is recommended that the user stores the BCD value 19 (0001,1001) in the location now, and on 1st January 2000, at 12:00:01 AM, updates it to the BCD value 20 (0010,0000). TIMEKEEPER devices that do not have a Century register, and that do not utilize the 16-byte register map definition, can still adopt the same methodology. Any address location that is convenient to the application can be used for storing the Century information. Note: All TIMEKEEPERS automatically allow for 31, 30, 29 and 28 day months (correctly adjusting for leap-years until the year 2100).
May 2000 1/2
AN923 - APPLICATION NOTE
If you have any questions or suggestions concerning the matters raised in this document, please send them to the following electronic mail addresses:
apps.nvram@ st.com ask.memory@ st.com
(for application support) (for general enquiries)
Please remember to include your name, company, location, telephone number and fax number.
Information furnished is believed to be accurate and reliable. However, STMicroelectronics assumes no responsibility for the consequences of use of such information nor for any infringement of patents or other rights of third parties which may result from its use. No license is granted by implication or otherwise under any patent or patent rights of STMicroelectronics. Specifications mentioned in this publication are subject to change without notice. This publication supersedes and replaces all information previously supplied. STMicroelectronics products are not authorized for use as critical components in life support devices or systems without express written approval of STMicroelectronics. 2000 STMicroelectronics - All Rights Reserved The ST logo is a registered trademark of STMicroelectronics. All other names are the property of their respective owners. STMicroelectronics GROUP OF COMPANIES Australia - Brazil - China - Finland - France - Germany - Hong Kong - India - Italy - Japan - Malaysia - Malta - Morocco - Singapore - Spain Sweden - Switzerland - United Kingdom - U.S.A. http://www.st.com
2/2
Document Number: 5227