製品概要
概要
The X-CUBE-MATTER Expansion Package features Matter support preintegrated on compatible STM32 microcontrollers. It is a reference implementation for the demonstration of Matter on STM32. It is ready for prototyping a Matter end-device or Matter bridge on a reference development platform. Refer to STMicroelectronics Matter wiki articles at wiki.st.com/stm32mcu for the supported STM32 platforms.
X-CUBE-MATTER is Matter precertified with the default dimmable light device type. However, it also provides other device types.
The Matter application project stores the device credentials and keys in the STM32 embedded flash memory, or in an external flash memory for which X-CUBE-MATTER provides a driver. Once provisioned, the security-sensitive data and operations remain in a secure partition, where they are not exposed to the user application. The Secure Boot process acts as a Root of Trust for the application before launching it. It takes care of the Secure Firmware Update once the user application has downloaded a new image.
The X-CUBE-MATTER Expansion Package embeds different sorts of open-source components:
- Matter SDK from the CSA
- Some other third-party components selected by STMicroelectronics (such as FreeRTOS™ kernel, Mbed TLS, and LwIP) are reintegrated
- Some components implemented by STMicroelectronics (such as the Bluetooth® LE, OpenThread, and Wi‑Fi® platform adaptation layers)
The OpenThread, Bluetooth® LE, and Wi‑Fi® stacks can be located on the application microcontroller in the case of a chipset solution. They can also be located on the coprocessor dedicated to the wireless stack. Refer to STMicroelectronics Matter wiki articles at wiki.st.com/stm32mcu for the software partitioning of each target platform.
The delivered application examples are part of the project. They are available as precompiled binaries for an out-of-the-box experience. The source codes are also available. They can be compiled with the supported IDEs. Refer to the wiki site for the detailed list of supported applications.
-
特徴
- Integration of Matter on compatible STM32 microcontrollers with examples of application for end-device and bridge Matter accessories
- Support for Matter SDK 1.5.0
- Support for Bluetooth® LE protocol stack for device commissioning
- Support for the Thread operational network
- Support for the Wi‑Fi® operational network
- Support for Ethernet as the bridge link to the access point or router
- Certified Bluetooth® LE protocol stack
- Precertified Thread 1.4 protocol stack
- Certified Wi‑Fi® protocol stack
- Support for the LwIP TCP/IP protocol stack
- Concurrent operational mode with Thread and Bluetooth® LE
- Concurrent operational mode with Wi‑Fi® and Bluetooth® LE
- FreeRTOS™ kernel
- Ready for CSA certification
- Support for on-demand provisioning service to install factory data including device attestation certificate (DAC)
- During Matter device manufacturing
- On the field
- Low power capable
- Security component (cryptographic library)
- Secure Boot and Secure Firmware Update over-the-air (OTA)
- Secure OTA with OEMiRoT using internal and external flash memory on STM32WBA6xxx wireless microcontrollers
- Secure OTA with SBSFU using internal flash memory on STM32U575xx microcontrollers
- Secure storage with Arm® TrustZone® enabled and TFM on STM32WBA6xxx wireless microcontrollers
- Drivers and libraries
- Project binary files provided for immediate demonstration