Join us in Nashville
“Dock” at our booth 502/504 to “encounter” our experts and discuss the latest innovations in radiation hardened ceramic and plastic products for Low Earth Orbit.
Featured demos
LVDS Driver for 2.5 V Logic
Showing our evaluation board for our new 2.5 V, 600 Mbps LVDS driver, demonstrating its optimized pinout for easy soldering onto the board. QML-V qualified with TID of 300 Krad with the receiver coming at the end of 2025.
Integrated Current Limiter
Our Integrated Current Limiter device pairs with a Rad-Hard Power-MOSFET to create a protection circuit for devices down the line.
LEO POL Buck Regulator
New LEO-Grade 12 V, 5 A plastic buck regulator for Point of Load applications has been released in 2025 for flight, with the additional capability of implementing current sharing with multiple out-of-phase devices.
12-Bit A/D Multiplex Converter
The RHFAD128 is a 12-Bit 8-Channel Analog-Digital Converter with an operating voltage of 12.7 V to 3.3 V, and will be present as a static demo to showcase the required external components and package size.
Register for NSREC
Join the industry's top technical experts in Space and Rad Hard. We look forward to meeting you.
日付
2025年 07月 14日 - 18日
場所
Nashville, TN
Register for NSREC
Join the industry's top technical experts in Space and Rad Hard. We look forward to meeting you.
2025年 07月 14日 - 18日
Nashville, TN
Register now!