Digi International is a leading global provider of IoT connectivity products, services, and embedded system-on-module (SOM) solutions. It helps companies create next-generation connected products and deploy and manage devices in demanding environments with high levels of security and reliability.
Since 1985, Digi has been a pioneer in wireless communication, forging the future for connected devices and responding to the needs of the people and enterprises that use them.
The Digi ConnectCore SOM solution provides a highly integrated hardware and software platform including wireless communication capabilities. Designed for rapid development and time-to-market they come with a full suite of tools and resources for scalability and ease of maintenance.
With robust, industrial grade hardware, integrated Digi TrustFence® security, the fully validated Digi Embedded Yocto Linux operating system and device management tools, Digi’s embedded solutions reduce the total cost of ownership and help catapult OEMs to market success.
Digi TrustFence®
All Digi ConnectCore SOMs incorporate Digi TrustFence®, a complete embedded security environment that OEMs can use to design security features into their products from the ground up. Regardless of an organization’s size, resources or security knowledge, developers can rely on Digi TrustFence for built-in security — without the cost and time needed to design from scratch. Digi TrustFence security features including Secure Boot, file system encryption, tamper detection, secure firmware updates and protected hardware ports, are fully implemented and ready to use, with complete documentation and step by step instructions.
Power Efficient
Low-power capabilities of Digi ConnectCore SOMs let developers optimize the power-consumption profile to fit their application needs. Digi ConnectCore SOMs offer best-in-class power management. They can operate in multiple power modes to minimize power consumption, which is especially important for battery powered devices. Digi Microcontroller Assist™ (MCA) gives users greater control of power levels.
Industrial Reliability
With an extended product warranty, Digi’s commitment to reliability and longevity is second to none. Digi ConnectCore SOMs are built exclusively with industrial-grade components and undergo rigorous thermal and shock testing to ensure that they can withstand harsh outdoor environments and temperature extremes of -40 to +85 C. Digi SOMs are duty-rated for continuous use — 24/7/365 — and designed for 10-year longevity, an especially important consideration for medical and industrial applications with lengthy regulatory approval cycles. Digi also provides support throughout the entire product lifecycle. Whenever there is a component change, Digi qualifies new components and updates the applicable software to support new features and functionality.
Wireless
Digi ConnectCore SOMs are pre-certified for global deployment, streamlining the country-by-country certification process for wireless products, which can often be lengthy and expensive. OEMs can reduce their development costs and realize a lower total cost of ownership (TCO) by leveraging this pre-certified wireless connectivity, as well as achieving faster time-to-market. All Digi SOMs have both a Wi-Fi and Bluetooth option on-board and are fully integrated with Digi XBee modules. Digi XBee modules support leading IoT standards like LTE cellular, mesh networking and long-range sub-GHz wireless connectivity.
Scalability
The range of compatible Digi ConnectCore products allows OEMs to future proof their designs while controlling manufacturing costs. If an application evolves and requires more processing power, developers can simply drop in a higher performance, footprint compatible, Digi ConnectCore module. The Digi ConnectCore Smart IOmux tool expedites the design process and ensures compatibility across SOM families.
Design Services and Support
Digi customer support begins with complete documentation and step-by-step instructions to streamline and simplify the work of designers and developers. The Digi Professional Services team offers skilled programming, application development, project planning and implementation services. In addition, Digi performs regular security audits to identify new and evolving threats and proactively communicates with customers regarding any known vulnerabilities.
In addition, Digi’s Wireless Design Services (WDS) team offers help with embedded / RF hardware and software design, certifications, and manufacturing support.
(#STM32MP1) (#STM32MPU)

Products and Services offered:
• Design Services
• Embedded Software
• Engineering Services
• Hardware Development Tools
• Hardware Integrated Devices
• Software Development Tools
Company Head Office address:
9350 Excelsior Blvd, Suite 700, 55343, Hopkins, Minnesota, United States
Company primary contact:
Contact
Company website:
www.digi.com
Partner Product | Description | Associated ST Products |
---|---|---|
Digi ConnectCore MP157 SOM | Intelligent and connected, secure embedded system-on-module based on STM32MP157C | STM32MP157 |
Partner Product | Description | Associated ST Products |
---|---|---|
Digi ConnectCore MP15 Development Kit | The Digi ConnectCore MP15 Development Kit delivers a complete development platform for embedded industrial products built on the ConnectCore MP15 SOM | STM32MP157 |
Partner Product | Description | Associated ST Products |
---|---|---|
Digi Embedded Yocto | Complete, open-source Linux solution based on the Yocto Project incl. TrustFence security, wireless integration, low power optimizations and more | STM32MP1 Series |
Digi TrustFence and Security Services | Digi TrustFence is a device-security framework that simplifies the process of securing connected devices | STM32MP1 Series |
Partner Product | Description | Associated ST Products |
---|---|---|
Support Services | The Digi support services team of technical engineers and online resources help you gain the most from your Digi products | STM32MP157 |
Partner Product | Description | Associated ST Products |
---|---|---|
Digi ConnectCore Smart IOmux Software Configuration Tool | Digi ConnectCore Smart IOmux helps to simplify pinout and Linux device tree configuration for Digi ConnectCore System-on-Module (SOM) designs | STM32MP157 |
Partner Product | Description | Associated ST Products |
---|---|---|
Digi ConnectCore Smart IOmux Hardware Development Tool | Digi ConnectCore Smart IOmux helps to simplify pinout and Linux device tree configuration for Digi ConnectCore System-on-Module (SOM) designs | STM32MP157 |
Partner Product | Description | Associated ST Products |
---|---|---|
Wireless Design Services | Digi Wireless Design Services (WDS) helps companies solve business problems by embedding wireless technologies to create innovative products | STM32MP1 Series |
Legal Disclaimer
In addition to the Terms of Use, ST Sales Terms & Conditions and Privacy Policy contained in this Web Site, the following terms and conditions apply to all STMicroelectronics partner programs.
Although STMicroelectronics has attempted to provide accurate information on the Web Site, STMicroelectronics assumes no responsibility for the accuracy of the information. All information provided by STMicroelectronics on this Web Site is provided “AS-IS”, with all faults and without warranty of any kind, whether expressed, implied or statutory. STMicroelectronics may change or discontinue its partner programs or its products or services at any time and without notice. Any mention of non-STMicroelectronics products or services is for information purposes only and does not constitute an endorsement by STMicroelectronics. The use of the word or term “partner or partners” on this Web Site does not indicate or imply the existence of any partnership or agency relationship or any legal or fiduciary relationship of any kind between STMicroelectronics and any other company or that such company is an affiliate of STMicroelectronics in any way. The partners in STMicroelectronics partner programs provide separate licenses for purchase or use of their products and/or services and related technology with STMicroelectronics devices. Contact the appropriate partner directly for licensing terms, price, support any other information on such partner’s product and/or services. The terms and conditions for such products and/or services may vary from partner to partner and are licensed directly and separately from such partner. STMicroelectronics makes no representations or warranties about the suitability of the products and services offered or provided by the partners and STMicroelectronics hereby disclaims all warranties and conditions, whether express, implied or statutory with respect to any product or services provided by the partners, including but not limited to any warranties and conditions of merchantability, fitness for a particular purpose, title, non-infringement or arising from a course of dealing, usage or trade practice. In no event shall STMicroelectronics be liable for any direct, indirect, incidental, special, exemplary, consequential or punitive damages or any damages whatsoever, including but not limited to loss of use, profit or revenue however caused and on any theory of liability, whether in contract, strict liability or tort (including negligence or otherwise) arising in any way out of or in connection with your participation in or your reliance of the partner program, your use or inability to use or purchase of products and/or services from the partners or the performance of such products and services, your relationship with the partner, your use or inability to use or reliance on STMicroelectronics portal or any information provided by STMicroelectronics therein, even if advised of the possibility of such damage. Links to third party Web Sites, when provided by STMicroelectronics, are not under the control of STMicroelectronics and STMicroelectronics is not responsible for any contents, materials, opinions, advice or statements or for the accuracy or reliability of any such contents and materials made on any linked site or any link contained in a linked site, or any changes or updates to such sites. STMicroelectronics is not responsible for any form of transmission received from any linked site, including but not limited to webcasting or audio transmission. Access to any linked site or any link contained in a linked site is at the user's own risk. STMicroelectronics is providing these links to you only as a convenience and the inclusion of any link does not imply any warranty (implied, express or otherwise) or any endorsement by STMicroelectronics of the third party Web Site.

You’re now leaving st.com and will be re-directed to our Partner’s website.
For the latest innovations and solutions from ST, sign up for our newsletters.