Embedded Software
Accompanied by excellent project management, embeX develops firmware and embedded software for our customers. The programs run highly efficiently on bare microcontrollers or as applications under operating systems such as embedded Linux. They scale from particularly compact, resource-optimized to complex code. Our focus is always on measuring, controlling, driving, communicating in real-time and using GUIs.
https://www.embex-engineering.com/en/competencies-technologies/embedded-software-development/
Hardware
embeX develops customised embedded electronics and power electronics up to 500 kW. The development is completely focused on the goals of our customers: Short time-to-market, long-term available components, use of standards, high reliability and low production costs. We also routinely implement EMC-optimised layouts as well as demanding requirements for explosion protection, functional safety and high availability.
https://www.embex-engineering.com/en/competencies-technologies/embedded-hardware-development/
Manufacturing
We offer to develop your product. From the moment your idea is born all the way to production at our production partner or in your own facility. With the zero series we transfer our development into the production.
https://www.embex-engineering.com/en/competencies-technologies/system-engineering/
Test
embeX develops, operates and supplies automated test and inspection systems having an own capacity of 800 m2 lab area.
We leverage a uniform platform, the embeX measurement platform MPL based on LabVIEW and TestStand, to enable efficient and flexible use. With the help of embeX MPL, we cover all phases of the product lifecycle with one platform: from use in pre-development and verification through to production and repair, after-sales and the development of product variants.
https://www.embex-engineering.com/en/competencies-technologies/measurement-test/
Certification
embeX develops products for international markets and carry out type testing to check and compare with applicable standards, directives and specifications. Of course we provide the complete development documentation in a form ready for approval. Our employees are in constant contact with all the well-known, accredited inspection bodies to prepare and support approvals for our customers with documented product tests.
https://www.embex-engineering.com/en/competencies-technologies/certification/
System Engineering
embeX supports its customers in designing the entire embedded system. Ranging from the field level up to the cloud and covering standards of regulated markets such as functional safety, cyber security and explosion protection with a strong focus on intrisic safety.
https://www.embex-engineering.com/en/competencies-technologies/system-engineering/
Functional Safety
embeX is the first company worldwide to receive a TÜV Rheinland certificate with highest Maturity Level 5 for its Functional Safety Management System (FSM). The company is the leading provider of development services in the area of functional safety covering measurement, drive, and control technology, medical engineering and for the associated control devices. Embedded systems ranging from SIL 1 to SIL 4, from PL a to PL e, from medical device class I to III. embeX advises and supports its customers in all issues relating to functional safety, when implementing a functional safety management system and during assessment and certification.
https://www.embex-engineering.com/en/competencies-technologies/functional-safety/
Embedded Security
embeX provides all consulting and design services to protect embedded devices against espionage, and Cyber attacks on data as well as intellectual property. embeX develops such systems in accordance with IEC 62443 up to the highest security level SL 4.
https://www.embex-engineering.com/en/competencies-technologies/embedded-security/
Safety and Security
Functionally safe control systems are typically devices of networks. Thus, their interfaces need to be protected against Cyber attacks.
https://www.embex-engineering.com/en/competencies-technologies/safety-security/
Explosion Protection
As a leading engineering service provider, embeX realises systems for potentially explosive environments. embeX is the only service provider in Europe that offers expertise on all types of ignition protection including intrinsic safety (Ex-i) and pressure resistant housings (Ex-d) from a single source. The services cover explosion protection against both gases and dust.
https://www.embex-engineering.com/en/competencies-technologies/explosion-protection-atex/
Proposed Services | Application SW, Embedded SW, Hardware, Manufacturing, Other, Test & certification |
Site |
ST Products |
---|